Part Number: C2000-GANG
Hi All,
A) Have to design VFD:
One HP max
AC Input : 220Vac/50Hz
Output : 220Vac three phase
Output frequency : 5Hz - 400Hz max
Need Auto-tune function in field, without any external computer
B) For example, delta electronics makes vfd, in which you press button for autotune , it will autotune vfd no need to connect external computer or device. Its self sufficient https://www.deltaww.com/en-US/products/AC-Motor-Drives/ALL/
C) Is there any solution, offered by you which has internal Auto-tune written?
or whats the closest solution that i can find?