Part Number: TMS320F28377D
Other Parts Discussed in Thread: TMDSDOCK28379D
I'm currently considering accessing an external memory area using the parallel bus with the C2000 series, and I have the following question:
Which of the following is the output logic (Hi/Lo) of the RNW pin?
CASE 1:
READ: Maintains Hi
WRITE: Emits a Low pulse with the same width as CS
CASE 2:
READ: Emits a Hi pulse with the same width as CS
WRITE: Maintains Low
CASE 3:
Other than the above (please advise)
Is this behavior common across the C2000 series?
For example, do the XR/W~ and EM1RNW pins function the same on the TMS320F283335 and TMS320F28377D?
Regards,
T. Mori