This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: ADS7028: Not able to write data through MOSI from F28377D

Part Number: TMS320F28377D
Other Parts Discussed in Thread: ADS7028

I am trying read data in ADS7028 in auto-seq mode. I have started developing to sending data to write on the ADS, however the below configuration, I wanted to check before connecting the control card ADS7028 SPI connector. 
Below is my code. 

#include "driverlib.h"
#include "device.h"

#define ADS_SPI_BASE    SPIC_BASE
#define ADS_CS_GPIO     53  // Manual Chip Select

#define OPCODE_WRITE    0x08
#define REG_ADDR        0x11
#define REG_DATA        0x01

// --- Prototypes ---
void InitSystem_And_GPIO(void);
void InitSPI_DebugMode(void);
void ADS_RegisterWrite(uint8_t regAddr, uint8_t data);

void main(void)
{
    // 1. Initialize System
    Device_init();
    Device_initGPIO();
    Interrupt_initModule();
    Interrupt_initVectorTable();

    // 2. Setup Pins
    InitSystem_And_GPIO();

    // 3. Setup SPI (1 MHz, 8-bit mode for 3-byte writes)
    InitSPI_DebugMode();

    // 4. Power Up Delay
    DEVICE_DELAY_US(5000);

    while(1)
    {

        ADS_RegisterWrite(0x11, 0x01);
        DEVICE_DELAY_US(50);
    }
}

void InitSystem_And_GPIO(void)
{
    GPIO_unlockPortConfig(GPIO_PORT_B, 0xFFFFFFFF);

    // Configure SPI-C Pins (GPIO 50, 51, 52)
    GPIO_setMasterCore(50, GPIO_CORE_CPU1);
    GPIO_setPinConfig(GPIO_50_SPISIMOC);
    GPIO_setPadConfig(50, GPIO_PIN_TYPE_PULLUP);
    GPIO_setQualificationMode(50, GPIO_QUAL_ASYNC);

    GPIO_setMasterCore(51, GPIO_CORE_CPU1);
    GPIO_setPinConfig(GPIO_51_SPISOMIC);
    GPIO_setPadConfig(51, GPIO_PIN_TYPE_PULLUP);
    GPIO_setQualificationMode(51, GPIO_QUAL_ASYNC);

    GPIO_setMasterCore(52, GPIO_CORE_CPU1);
    GPIO_setPinConfig(GPIO_52_SPICLKC);
    GPIO_setPadConfig(52, GPIO_PIN_TYPE_PULLUP);
    GPIO_setQualificationMode(52, GPIO_QUAL_ASYNC);

    // Configure CS Pin (GPIO 53) as Manual Output
    GPIO_setMasterCore(53, GPIO_CORE_CPU1);
    GPIO_setPinConfig(GPIO_53_GPIO53);
    GPIO_setDirectionMode(53, GPIO_DIR_MODE_OUT);
    GPIO_writePin(53, 1); // Start High
}

void InitSPI_DebugMode(void)
{
    SPI_disableModule(ADS_SPI_BASE);

    // Config: 1 MHz, 8-bit Data Size, Mode 0 (Polarity 0, Phase 0)
    // We use 8-bit size so we can send Opcode(8) + Addr(8) + Data(8)
    SPI_setConfig(ADS_SPI_BASE, DEVICE_LSPCLK_FREQ, SPI_PROT_POL0PHA1,
                  SPI_MODE_MASTER, 1000000, 8);

    SPI_disableLoopback(ADS_SPI_BASE);
    SPI_setEmulationMode(ADS_SPI_BASE, SPI_EMULATION_FREE_RUN);

    // Enable FIFO (Helps buffer the 3 bytes)
   SPI_enableFIFO(ADS_SPI_BASE);

    SPI_enableModule(ADS_SPI_BASE);
}

void ADS_RegisterWrite(uint8_t regAddr, uint8_t data)
{
    GPIO_writePin(ADS_CS_GPIO, 0);
    DEVICE_DELAY_US(2);

    GPIO_writePin(ADS_CS_GPIO, 0);
    DEVICE_DELAY_US(2);  // t_CSSC delay

    // Send all 3 bytes
    SPI_writeDataBlockingFIFO(ADS_SPI_BASE, OPCODE_WRITE);   // Write command
    SPI_writeDataBlockingFIFO(ADS_SPI_BASE, regAddr);        // Register address
    SPI_writeDataBlockingFIFO(ADS_SPI_BASE, data);           // Data

    // Wait for transmission to complete
    // Check if SPI is still busy
    while(SPI_isBusy(ADS_SPI_BASE)) {}

    DEVICE_DELAY_US(20);
    GPIO_writePin(ADS_CS_GPIO, 1);
    DEVICE_DELAY_US(2);
}


1. Clk signal
2. MOSI

3. CS
There is no pull up in the hardware for any signal. MOSI should generate signal bits in within the clock cycle, right? 

  • Hi Souradeep, 

    The sample code given above looks correct. Can you configure a different set of pins or SPI instance and check if that works? 
    If you are using a Control Card, you can use the pins mentioned in the image below:

    Regards, 
    Pranav Siddappa