Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: In ram command file , how to increase data section size

Part Number: TMS320F28379D

Hi Sir,

How to increase data section size . While building program ,I am getting below error message,

[110]<Linking>
[111]"../2837xD_RAM_lnk_cpu1.cmd", line 91: error #10099-D: program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section. run placement with alignment/blocking fails for section ".data" size 0xa0 page 1.  Available memory ranges:
[112]   RAMLS5       size: 0x800        unused: 0xa6         max hole: 0xa6
[113]error #10010: errors encountered during linking; "integrated_code__pll_verified.out" not built

Thanks and Regards,

Prashant Gugle

  • Hi Prashant,

    Can you share the linker cmd file for further analysis?

    The memories allocated to .data section is not enough to accommodate the entire data, so we need to add additional memory section to fill the data.

    Please use GS0 RAM for the data section and check if it resolves your issue.

    .data            : > RAMGS0,    PAGE = 1

    Thanks

    Aswin

  • Hi Aswin,

    Please find the attached linker command file for your analysis.

    MEMORY
    {
    PAGE 0 :
       /* BEGIN is used for the "boot to SARAM" bootloader mode   */
    
       BEGIN            : origin = 0x000000, length = 0x000002
       RAMM0            : origin = 0x000123, length = 0x0002DD
       RAMD0            : origin = 0x00B000, length = 0x000800
       RAMLS0           : origin = 0x008000, length = 0x000800
       RAMLS1           : origin = 0x008800, length = 0x000800
       RAMLS2           : origin = 0x009000, length = 0x000800
       RAMLS3           : origin = 0x009800, length = 0x000800
       RAMLS4           : origin = 0x00A000, length = 0x000800
       RESET            : origin = 0x3FFFC0, length = 0x000002
    
      /* Flash sectors */
       FLASHA           : origin = 0x080002, length = 0x001FFE	/* on-chip Flash */
       FLASHB           : origin = 0x082000, length = 0x002000	/* on-chip Flash */
       FLASHC           : origin = 0x084000, length = 0x002000	/* on-chip Flash */
       FLASHD           : origin = 0x086000, length = 0x002000	/* on-chip Flash */
       FLASHE           : origin = 0x088000, length = 0x008000	/* on-chip Flash */
       FLASHF           : origin = 0x090000, length = 0x008000	/* on-chip Flash */
       FLASHG           : origin = 0x098000, length = 0x008000	/* on-chip Flash */
       FLASHH           : origin = 0x0A0000, length = 0x008000	/* on-chip Flash */
       FLASHI           : origin = 0x0A8000, length = 0x008000	/* on-chip Flash */
       FLASHJ           : origin = 0x0B0000, length = 0x008000	/* on-chip Flash */
       FLASHK           : origin = 0x0B8000, length = 0x002000	/* on-chip Flash */
       FLASHL           : origin = 0x0BA000, length = 0x002000	/* on-chip Flash */
       FLASHM           : origin = 0x0BC000, length = 0x002000	/* on-chip Flash */
       FLASHN           : origin = 0x0BE000, length = 0x001FF0	/* on-chip Flash */
    
    //   FLASHN_RSVD     : origin = 0x0BFFF0, length = 0x000010    /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
    
    PAGE 1 :
    
       BOOT_RSVD       : origin = 0x000002, length = 0x000121     /* Part of M0, BOOT rom will use this for stack */
       RAMM1           : origin = 0x000400, length = 0x0003F8     /* on-chip RAM block M1 */
    //   RAMM1_RSVD      : origin = 0x0007F8, length = 0x000008     /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
       RAMD1           : origin = 0x00B800, length = 0x000800
    
       RAMLS5      : origin = 0x00A800, length = 0x000800
    
       RAMGS0      : origin = 0x00C000, length = 0x001000
       RAMGS1      : origin = 0x00D000, length = 0x001000
       RAMGS2      : origin = 0x00E000, length = 0x001000
       RAMGS3      : origin = 0x00F000, length = 0x001000
       RAMGS4      : origin = 0x010000, length = 0x001000
       RAMGS5      : origin = 0x011000, length = 0x001000
       RAMGS6      : origin = 0x012000, length = 0x001000
       RAMGS7      : origin = 0x013000, length = 0x001000
       RAMGS8      : origin = 0x014000, length = 0x001000
       RAMGS9      : origin = 0x015000, length = 0x001000
       RAMGS10     : origin = 0x016000, length = 0x001000
    
    //   RAMGS11     : origin = 0x017000, length = 0x000FF8   /* Uncomment for F28374D, F28376D devices */
    
    //   RAMGS11_RSVD : origin = 0x017FF8, length = 0x000008    /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
    
       RAMGS11     : origin = 0x017000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
       RAMGS12     : origin = 0x018000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
       RAMGS13     : origin = 0x019000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
       RAMGS14     : origin = 0x01A000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
       RAMGS15     : origin = 0x01B000, length = 0x000FF8     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
       
    //   RAMGS15_RSVD : origin = 0x01BFF8, length = 0x000008    /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
                                                                /* Only on F28379D, F28377D, F28375D devices. Remove line on other devices. */
    
       CPU2TOCPU1RAM   : origin = 0x03F800, length = 0x000400
       CPU1TOCPU2RAM   : origin = 0x03FC00, length = 0x000400
    
       CANA_MSG_RAM     : origin = 0x049000, length = 0x000800
       CANB_MSG_RAM     : origin = 0x04B000, length = 0x000800
    }
    
    
    SECTIONS
    {
       codestart        : > BEGIN,     PAGE = 0
       .text            : >> RAMGS0 | RAMGS1 | RAMGS2 | RAMGS3, PAGE = 1
       .cinit           : > RAMM0,     PAGE = 0
       .switch          : > RAMM0,     PAGE = 0
       .reset           : > RESET,     PAGE = 0, TYPE = DSECT /* not used, */
       .stack           : > RAMM1,     PAGE = 1
    
    #if defined(__TI_EABI__)
       .bss             : > RAMLS5,    PAGE = 1
       .bss:output      : > RAMLS3,    PAGE = 0
       .init_array      : > RAMM0,     PAGE = 0
       .const           : > RAMLS5,    PAGE = 1
       .data            : > RAMLS5,    PAGE = 1     
       .sysmem          : > RAMLS5,    PAGE = 1
    #else
       .pinit           : > RAMM0,     PAGE = 0
       .ebss            : > RAMLS5,    PAGE = 1
       .econst          : > RAMLS5,    PAGE = 1
       .esysmem         : > RAMLS5,    PAGE = 1
    #endif
    	/* Digital Controller Library functions */
    	dclfuncs		     : > RAMLS4,		PAGE = 0
    	dcl32funcs		  : > RAMLS4,		PAGE = 0
    
       Filter_RegsFile  : > RAMGS0,    PAGE = 1
    
    
       ramgs0           : > RAMGS0,    PAGE = 1
       ramgs1           : > RAMGS1,    PAGE = 1
    
    #ifdef __TI_COMPILER_VERSION__
       #if __TI_COMPILER_VERSION__ >= 15009000
        .TI.ramfunc : {} > RAMM0,      PAGE = 0
       #else
        ramfuncs    : > RAMM0      PAGE = 0   
       #endif
    #endif
    
       /* The following section definitions are required when using the IPC API Drivers */
        GROUP : > CPU1TOCPU2RAM, PAGE = 1
        {
            PUTBUFFER
            PUTWRITEIDX
            GETREADIDX
        }
    
        GROUP : > CPU2TOCPU1RAM, PAGE = 1
        {
            GETBUFFER :    TYPE = DSECT
            GETWRITEIDX :  TYPE = DSECT
            PUTREADIDX :   TYPE = DSECT
        }
    
        /* The following section definition are for SDFM examples */
       Filter1_RegsFile : > RAMGS1, PAGE = 1, fill=0x1111
       Filter2_RegsFile : > RAMGS2, PAGE = 1, fill=0x2222
       Filter3_RegsFile : > RAMGS3, PAGE = 1, fill=0x3333
       Filter4_RegsFile : > RAMGS4, PAGE = 1, fill=0x4444
       Difference_RegsFile : >RAMGS5,   PAGE = 1, fill=0x3333
    }
    
    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */
    

  • Hi Prashant,

    Please use GS0 RAM for the data section and check if it resolves your issue.

    .data            : > RAMGS0,    PAGE = 1

    Thanks

    Aswin

  • Hi Aswin,

    Even when I used RAMGS0 for .text section 

      .text            : >> RAMGS0 | RAMGS1 | RAMGS2 | RAMGS3, PAGE = 1

    still it is okay to use for .data section?

    Actually, I used RAMGS0 for data section and it builds without errors.

    Thanks and Regards,

    Prashant Gugle