Part Number: CODECOMPOSER
I can't able to access the uint8_t type in empty bitfield project

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Type names like int16_t and uint16_t are defined in the standard RTS header file stdint.h. Because C28x has no 8-bit wide type, the name uint8_t is not present in stdint.h. I cannot say why the type name uint8_t is used in the file empty_bitfield_main.c
Thanks and regards,
-George