Part Number: LAUNCHXL-F280039C
Other Parts Discussed in Thread: C2000WARE
Hi,
I'm using LAUNCHXL-F280039C board with CCS V20.4.0.13, and also installed C2000Ware_6_00_01_00.
I loaded and ran Debug on an example project, led_ex1_blinky, without any issue on the board. But when I ran Debug on other example project, sci_ex4_stdout_redirect, I got the following error:
"IcePick_C_0: Error connecting to the target: (Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 20.4.0.3756) "
I connected the board through a USB cable to my PC. And I disconnected/reconnected the board and restarted CCS multiple times. And also tried to reset the board.
These two examples come from C2000Ware_6_00_01_00.
What's the cause of the problem and how to fix it?
Thanks
David