Part Number: TMS320F28377D
Hi Team,
I am using TMS320F28377DGWTEP BGA package. It is recommended in the datasheet to place total minimum 20uF capacitor near each pin of VDD for 1.2V supply. There are 14 pins and I have such 14 capacitors with value of 2.2uF. The package I am using is 0402. There is difficultly in placing all 14 capacitors near the pin VDD.
- If you have any layout reference to show how to place all capacitors near VDD pin on 1.2V supply please share the same.
- Currently I am using all 2.2uF capacitors on VDD, Is there any need of using 0.01uF or 0.1uF high frequency capacitor on VDD pin along with some 2.2uF, 10uF etc.
- Can we reduce package to 0201 to accommodate all 2.2uF capacitors near BGA pin?
Please provide your inputs.
Thanks,
Namita