Part Number: XDS110ISO-EVM
Hi,
I have purchased an XDS110ISO-EVM probe, because non-isolated probe keep disconnecting during debug due to common mode noise. However, I can't get it to work.
I am using an F280033 target on a custom board. Programming the target works perfectly using a regular non-isolated XDS110 probe.
However, when using the XDS110ISO-EVM probe (exact same project, exact same ccxml file), I get the following error message :

Which is strange, because the probe is correctly detected by windows :

When I go into advanced mode and try to test the connexion, I get the following result :
-----[Print the board config pathname(s)]------------------------------------
C:\Users\A0564~1.THU\AppData\Local\TEXASI~1\
CCS\CCS_20_4\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100/110/510 class product.
This utility will load the adapter 'jioxds110.dll'.
The library build date was 'Nov 20 2025'.
The library build time was '14:44:07'.
The library package version is '20.4.0.3756'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '5' (0x00000005).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the XDS110 with USB interface.
The link from controller to target is direct (without cable).
The software is configured for XDS110 features.
The controller cannot monitor the value on the EMU[0] pin.
The controller cannot monitor the value on the EMU[1] pin.
The controller cannot control the timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '0' (0x0000).
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-233' (0xffffff17).
The title is 'SC_ERR_PATH_BROKEN'.
The explanation is:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.
Again, no issue with a regular XDS110 probe.
Please help me get this to work.
Thanks in advance,
Adrien