Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CODECOMPOSER: CCS incorrect path on project import

Part Number: CODECOMPOSER
Other Parts Discussed in Thread: C2000WARE

Hi Team,

Posting on behalf of our customer.

When I try to import a new project  using project wizard (e.g. gpio_toggle with LAUNCHXL F28069M) with CCS 20.4.0.13__1.10.0 (macOS 15.7.3) I get the following error: 

\Specified location is not accessible: '/Users/szymon/ti/C2000Ware_6_00_01_00/C2000Ware_6_00_01_00/device_support/f2806x/examples/c28/gpio_toggle'

Note the duplicated C2000Ware_6_00_01_00 part. Import fails because of this error. C2000Ware path is correctly discovered in CCS settings. 

I noticed this is only a problem when CCS installs C2000ware on its own. It installs it in /Users/szymon/ti/C2000Ware_6_00_01_00 and it looks in /Users/szymon/ti/C2000Ware_6_00_01_00/C2000Ware_6_00_01_00.

I deleted that installation and installed C2000Ware from a standalone installer in the default folder: /Applications/ti/c2000/C2000Ware_6_00_01_00/ and the import worked correctly.

Steps to reproduce:
1. Install CCS 20.4 on a clean machine
2. Start the project import
3. CCS installs C2000Ware in the user folder /Users/username/ti/
4. CCS fails to import the project due to duplicated C2000 part of the path string

Regards,

Danilo