Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: Watchdog implementation method - F28388D

Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE

HELLO

  1. Is it possible to distinguish cpu1(master core) & cpu2 (Dependent core) 
  2. Can cpu1 and cpu2 handshake with each other?
  3. I want to reset all of CPU1, CPU2 & CM when handshake between CPU1 and CPU2 fails. How should I reset them? Please let me know both HW and SW methods.
  4. I'm looking to buy a USB TO JTAG debugger for the F28388D. Which model should I buy?

THANK YOU.

 

  • Hi,

    Is it possible to distinguish cpu1(master core) & cpu2 (Dependent core) 

    Can cpu1 and cpu2 handshake with each other?

    Yes Use IPC, refer to reference manual for more details

    I want to reset all of CPU1, CPU2 & CM when handshake between CPU1 and CPU2 fails. How should I reset them? Please let me know both HW and SW methods.

    Yes you can use WD to trigger XRSn. refer to c2000ware example to understand WD implementation.

    Software way would to use below register

    I'm looking to buy a USB TO JTAG debugger for the F28388D. Which model should I buy?

    Would suggest to start with XDS110 or 200.

    Thanks