This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3435-Q1: WD-EN Pin control during flashing of MCU

Part Number: TPS3435-Q1

Hi...

We're planning to use TPS3435CECAJDDFRQ1 in our application to control the reset pin of TMS320S28377SPTPT.

When the MCU enters the flash mode, then it can't provide WDI which would lead to WDT pulling the reset of MCU down, continuously.

For this, we had planned to connect the TRST pin through a BJT to the WD-EN pin so that when the MCU is working (TRST-0), WD-EN would be high & WDT will work as usual.

When TRST is 1, MCU enters flash mode & at that time, the WD-EN will be made zero i.e. WDT will not have control over the MCU reset during flashing.

Kindly let me know your views on this implementation.

Best Regards,

Prahaladh S