Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28379D: Help with Component selection

Part Number: LAUNCHXL-F28379D

Hi,

I got LAUNCHXL-F28379D EvlBoard. I wanted a Ethernet Port added to this, so i can connect it to my PC and have a custom software to monitor real-time V&I parameter monitoring; Can you suggest which one should I get and how should i connect it to this board? Does wiznet w5500(W5500 ETHERNET SHIELD or WIZnet W5500-io or USR-ES)1 is compatable with this board?

It would be great if you could provide specific component for this. 

Thank you!


 

Regards,

F Prem.

  • Hi F Prem,

    I unfortunately do not have familiarity with wiznet. If you have questions specific to this device's functionality and the SPI module implementation, I'd be able to help with issues you run into when setting up your program. Otherwise, I will close this thread for now.

    Best Regards,

    Allison