This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Documentation on DEVICECNF

Hi

We are using the TMS320x28069 and I am starting to work with the USB.  The documentation for setting PLL2 refers to DEVICECNF.SYSCLK2DIVDIS (see figure 1-28 in the December update of the technical reference manual, SPRUH18C).  However the description of this register (Table 1-109) does not mention this field.  Are we allowed to change it, which bit positions is it, and what are the allowed values?

Thanks

 

 

  • I'd like to add a couple of other observations regarding the documentation.

    Table 1-27 refers to a PLL2CR register but such a register does not seem to exist.

    Also there is a copy/paste error in Table 1-29 in which the Bit and Field columns should refer to Bit 0,  PLL2LOCKS.