This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6655: NOR FLASH UPGRADE ISSUE IN NOR BOOT MODE

Part Number: TMS320C6655
Other Parts Discussed in Thread: SYSBIOS

Hi,

We are using TMS320C6655 processor with MT25QU128ABA8EESF-0SIT nor flash in our design to boot processor code from this Nor Flash. Upgrade is working consistently in NO BOOT MODE. 

  But we have to do remote upgrade in field without jtags, So we have to do it NOR BOOT MODE only. 

We are using norwriter.c with processor code. Nor writer version is 01.00.00.04. Nor read verify fails in  sector 0 only, MSB bit shift happens. Read verify do not fail in other sectors.

  Request to help fix this issue.