This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: Faster MCU with more memory

Part Number: TMS320F28377S
Other Parts Discussed in Thread: TMS320F28377D, F29H850TU, AM263P4

Hi Team,

Posting on behalf of our customer.

I will share this E2E post to our customer so he can reply when needed.

Our customer will start a new project and would like to know if we have a MCU that is faster and or has more memory than TMS320F28377S. I have checked our C2000 product portfolio but it seems that the TMS320F28377S is the fastest one under its category.  

Regards,

Danilo

  • Hello Danilo, 

    I'd suggest a couple of options below. 

    1) TMS320F28377D which has one more C28x DSP + CLA than TMS320F28377S, doubling processing capability. We also have TMSP320F28377D-EP for extended temperature range targeting aerospace. 

    2) F29H850TU which has 3 next-gen C29x DSP cores at 200MHz. Each C29x offers more than 2x performance than C28x DSP. The device also has large flash and RAM. 

    3) AM263P4 which has 4 Cortex-R5F core running at 500MHz, which is not a C2000 device though. 

     Pls let me know if you have any additional questions. 

    Best Regards, 
    Michael