This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28377D-SEP: I2C SLAVE ADDRESS NOT DETECT IN THE PROCESSOR CARD

Part Number: F28377D-SEP
Other Parts Discussed in Thread: C2000WARE

The F28379D controller has two I²C interfaces: I2C0 and I2C1.
On I2C0, an EEPROM and RTC are connected, and this interface is working fine.

Now, I am trying to connect I2C1 to the processor via the backplane. I have configured the slave address as 0x4A, but I am not sure whether this address is correct or not. Here, the F28379D is configured as an I²C slave for the Processor card.

However, the I²C slave address is not detected on the processor card. I want to confirm whether configuring the F28379D as an I²C slave will work in this setup or not.
Whether my slave address is correct or not ?
Please check my below code.


#define I2C1_SLAVE_ADDR  0x31   // choose any free 7-bit address


void i2c1_slave_init(void)
{
    // Disable module before config
    I2C_disableModule(I2CB_BASE);

    // Init clock (speed irrelevant for slave, but required)
    I2C_initController(I2CB_BASE,
                       DEVICE_SYSCLK_FREQ,
                       100000,
                       I2C_DUTYCYCLE_50);

    //  Configure as SLAVE
    I2C_setConfig(I2CB_BASE, I2C_SLAVE_RECEIVE_MODE);

    //  Set OWN slave address (this is what master scans)
    I2C_setOwnAddress(I2CB_BASE, I2C1_SLAVE_ADDR);

    // 7-bit addressing
    I2C_setAddressMode(I2CB_BASE, I2C_ADDR_MODE_7BITS);

    // Standard 8-bit data
    I2C_setBitCount(I2CB_BASE, I2C_BITCOUNT_8);

    // Disable loopback
    I2C_disableLoopback(I2CB_BASE);

    // FIFO not required since no data transfer
    I2C_disableFIFO(I2CB_BASE);

    // Clear pending status
    I2C_clearStatus(I2CB_BASE,
                    I2C_STS_NO_ACK |
                    I2C_STS_ARB_LOST |
                    I2C_STS_STOP_CONDITION);

    // Enable module
    I2C_enableModule(I2CB_BASE);
}

 

call the below function in main

i2c1_slave_init();

  • Hi Saravanan,

    Now, I am trying to connect I2C1 to the processor via the backplane. I have configured the slave address as 0x4A, but I am not sure whether this address is correct or not. Here, the F28379D is configured as an I²C slave for the Processor card.
    #define I2C1_SLAVE_ADDR  0x31   // choose any free 7-bit address

     You have mentioned here the address is 0x4A, but your code configures it as 0x31. Configs look okay, except you don't need the following in target mode:

    // Init clock (speed irrelevant for slave, but required)
        I2C_initController(I2CB_BASE,
                           DEVICE_SYSCLK_FREQ,
                           100000,
                           I2C_DUTYCYCLE_50);

    Use only I2C_setConfig() instead.

    In addition, why is the I2C_INT_ADDR_TARGET interrupt not used? Refer to C2000WARE examples for how to configure controller vs. target I2C mode.

    Best Regards,

    Aishwarya