Other Parts Discussed in Thread: CONTROLSUITE
In build level 4 of the Sensored FOC guide, the current model is to be verified. It states (page 31):
-Compare Curmod1.Theta with rg1.Out via PWMDAC or CCS graph window. They should be identical with a small phase shift.
This was not the case for me. At a speedRef of .25 PU (Base Frequency = 120), rg1.Out was 30 Hz, but cm1.Theta was 45Hz. Similarly, at speedRef = .3 PU , rg1.Out was 36Hz. , and cm1.Theta was at 50Hz. At speedRef = .4PU, rg1.Out was 48Hz, but cm1.Theta was 60Hz. This was all measured using the PWMDACs and a scope.
It seemed as I increased the speed, the error between the two decreased, but was still off significantly. Also of note were the strange 'blips' that showed up in cm1.Theta on the CCS graph. That is, there would be a normal looking triangle wave, with a random 'half triangle' or a very distorted triangle appearing somewhere in the graph. I can post a screen shot of this if needed.
There isn't really anything said in the FOC document about how to correct this... it just states to verify it. Any help would be appreciated.
Thanks!