Part Number: TMS320F280039C
Other Parts Discussed in Thread: C2000WARE
I have a query regarding the F28003x processor. I have its Launchpad version.
I am using the onboard crystal oscillator of 20Mhz to create SYSCLK of 120MHz.
Compared to F2837xD Launchpad which has a SYSCLK of 200Mhz, I see it takes longer duration to execute the same set of instructions, twice or thrice even, on F28003x compared to F2837xD.
I need to understand whether I am missing something with the processor, whether some setting is causing significant time to execute instructions. I tried finding similar cases but couldn't on this platform so I need to check if someone here has seen such issues in the past in this processor, or some other processor in general has used long time to execute instructions and by changing some setting it started working fine.
If there are certain instructions/functions that can be used to check the time it takes to execute them and see if something is wrong by comparing with already benchmarked results of F28003x, with the execution, that would be helpful as well.