This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800156-Q1: Motor start sensorless with instaspin in EV compressor application

Part Number: TMS320F2800156-Q1

Hi 

I find one issue with motor start under full load with instaspin fast enabled.

The motor stalls at 2Hz, which equals to the force angle, is it stuck in open loop?

What will cause this issue?

The phase current is as below showing.

For 1st start, motor seems not go to the close loop ,and stuck at open loop with 2Hz, and the phase current is only 20A, not reach the max start current 50A.

For 2nd start, it will go to 600rpm and than drop to 2Hz and wait for 1s , than go to the target speed.

Application is 800V EV compressor with a 8P12S IPMSM, and test with liquid refrigerant in the compressor.

Regards

Wu