This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P650DH: Integrate secure boot beyond 16KB to existing bootloader (>16KB)

Part Number: TMS320F28P650DH

Hi Experts,

My customer is integraing secure boot features to their existing projects.

As we know the boot rom only supports secure boot for the first 16K and the memory beyoud 16K need to be covered by the SW within the first 16K.

However, my customer's bootloader is already larger than 16K, which is around 30K-40K.

In this case, how to integrate secure boot features into the existing projects?

Is it possible to isolated the secure boot features from the rest of the bootloaders and put it the first 16K? 

Regards,

Hang