This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Controller Card FTDI or XDS110 ???

Part Number: TMS320F28379D

Hi I am developing this Control card using TMS320F28379DPTPQ  chip (176 pin)

 

While developing the Card , I am taking help from the reference design of  LaunchXL_F28379D. It has a FTDI IC on the inside for USB-JTAG Debugging (  P02_XDS100v2 ) . I was thinking of not using it and directly connect the external XDS100V2 connector to use it for debugging . 

While researching I found that TI has discontinued selling XDS100V2 and have upgraded to XDS110.

I would like to know the better suited option . I am on a tight timeline . If we go with XDS110 what changes do i need to have ? 

TDO TDI TRST TMS TCK .... We just connect the new XDS110 to these and it works just like XDS110V2. 

Or would you recommend putting the FTDI on the control card itself and usi a mini usb to debug it ?