This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F29H85X-SOM-EVM: Secure Boot flow of F29h85x

Part Number: F29H85X-SOM-EVM

Hi,

  • If updating the key paths in devconfig.mak (TI-FS), imports.mak (F29 – CLI build), and makefiles.def (F29 – CCS build) is sufficient to create an HS-SE image, but encryption is disabled in the post-build steps, how will the images be encrypted?
  • When a flash-based application is loaded in HS-SE mode, will the application be decrypted and then written to the flash?
  • How can I update the software revision of the SBL, Application, and HSMRt images?

Regards,

Shashank