This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P550SG: [FAQ]: F28P550 ADC external reference configuration in sysconfig

Part Number: TMS320F28P550SG
Other Parts Discussed in Thread: SYSCONFIG

Hi team,

There is an ADC reference configuration bug in the sysconfig. When I select "Analog reference" as "external", there is no button used to configure "ADC_REFERENCE_3_3V" or "ADC_REFERENCE_2_5V"

image.png

  • To configure full-scale external ADC VREFHI (0V- VREFHI) in syscfg following steps needs to be followed:

    1. Select " internal' and "ADC_REFERENCE_2_5V" 

    image.png

    2. Switch " internal' to "external". This way, the external VREFHI is enabled. Please give another check in generated files board.c to make sure change applied correctly.

    image.png