This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: Inquiry on Suitability of TMS320F28377s for Application

Part Number: TMS320F28377S

To Whom it may concern

I am currently working with the TMS320F28377s (176 pins) and would like to confirm whether it is suitable for my application under the following conditions:

1. SPI Interfaces
   - SPI-A: micro SD card
   - SPI-B: multi-slave configuration
     * ADC (AD7734: 24-bit, 4 channels) – 3 units, all channels set to 100 Hz sampling rate
     * DAC (AD5064: 16-bit, 4 channels) – 1 unit
   - SPI-C:
     * ADC (AD7172: 24-bit, 2 channels) – 1 unit, all channels set to 400 Hz sampling rate

2. I2C Interface
   - RTC (m41t82)

3. UART x 4
   - Real-time message communication with other chips
   - Each port uses a 2048-word buffer

4. Algorithms
   - Temperature PID control: 4 channels
   - Flow PID control: 8 channels

5. SD Card File Storage
   - Multiple files:
     * Calibration-related files
     * Log files
     * Measurement data files

6. Important Data Storage
   - Using 2 Flash sectors

Could you please advise whether the TMS320F28377s is appropriate for these requirements, particularly in terms of memory usage and real-time processing capability? Any recommendations or insights would be greatly appreciated.

Best regards,
sjkim