This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI,
I ve already connecect F28335 eZdsp CCStudio v3.3 to Matlab matlab r2009a, it works the link, but when I tried to simulate a demo "ADC-PWM synchronization via
ADC interrup" (the program is built and loaded into the DSP but i can not see any PWM). I also tried to simulate " Real -Time data exchange via DTDX" but
I can not see any sine wave in the script. I think that it should be sofware incopatibility
I have the following programs
WINXP SP3
CCStudio v3.3
matlab r2009a (matlab7.8)(simulink7.3)
enbedded IDE link CC3.4
real time workshop 7.3
real time workshop embedded coder 5.3
target support package TC2 3.2
bios_5_33_03
if somebody could help me , i appreciate it becauce i ve been trying to solve this problem so long.
cheers
David