This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28386D: XRSn reset is not visible on the BOOT ROM STATUS

Part Number: TMS320F28386D
Other Parts Discussed in Thread: C2000WARE

Hello,

-I have my XRSn reset path, connected to a PMIC chip and I tried doing a test in which I force ESM reset by the PMIC chip and in the next startup I check the PMIC registers and the BOOTROM status to confirm that the reset caused is ESM through XRSn.

-The PMIC registers confirm that ESM reset was triggered, actual reset occured but when I check the BOOTROM Status I don't see the XRSn flag set and only the All handled Resets flag is set.

-The BOOTROM Status value is 0x80011002

-This test is only executed after cold starts, and it fails very very sporadically.