Part Number: TMS320F28375S
I'm working on a project with the TMS320F28375SZWTT where we're using GPIO104, Pin J2, EQEP3A to count pulses from an external high speed device. I understand that the max input frequency for the eQEP module, in theory, is SYSCLK/2, however, there must be some setup and hold requirement for the sysclk qualification that would reduce the max frequency a bit? What is the worst case setup and hold we would see on the pins which would allow us to calculate the realistic lower bound for eQEP Fmax?