This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F29H859TU-Q1: Can use TPS62901 to supply 1.25V?

Part Number: F29H859TU-Q1
Other Parts Discussed in Thread: TPS62902, TPS62901

Hi team,

I ask this for my customer.

My customer is desgin F29P329SM1RFSQ1 schematic, and they find in our SOM board, we use TPS62902(max current is 2A) to supply 1.25V current

image.png

Actually, for F29P32, the max 1.25V current is 760mA, and even for F29H85, they max 1.25V current is 820mA

image.png 

so they want to check if they can use TPS62901(max current is 1A) to supply 1.25V current?