Part Number: TMS320F28075
HI guys, This is weird. I'm using TMS320F28075 LQFP 176Pin on standalone board and suddenly codestart stopped working. In the past months it's been working fine but now no go.
I write ASM code using CCS12.8.1 and download my assembler code to the MCU and it would always run fine. Power off then on and the MCU would start exactly how it should with no problems.
Now I download my code, power off and then on and the MCU will not run. Very Strange.
I then loaded up CCS20.4.1 and wrote a small ASM program ( BLINKY ) and downloaded the code to the MCU, powered off and then on and the MCU would startup fine and LED's on PORTA would start flashing but using CCS12.8.1 it just won't run after powering off and then on again.
I haven't changed anything in CCS12.8.1, just written ASM code. The MCU works fine using CCS20.4.1 so its definatly something to do with CCS12.8.1.
Oh, I'm using an iMac with OS 15.7.1 Sequoia.
Any suggestions would be very much appreciated.
Thanks guys, Peter.