This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: Disassembly is not align with customer code

Part Number: TMS320F28377S

Hi Experts

Customer reports an issue that the memory address in disassembly is not align with their code, refer to the picture below, the 1st mov32 address in disassembly line 91213 is 0x3e stands for the f32claVarFilter_wt, then the second address in disassembly line 91217 should be 0x44 stands for f32claVarFilter_OutMax, but the address shows in the window is 0x4, then 0x6 is also wrong. those issues leadsto the data written in the wrong address. could you please kindly check the issues?

image.png

Thanks

Joe