This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039C: SPI TX data abnomal

Part Number: TMS320F280039C

Hello,

We are using the TMS320F280039C as Slave Mode to communicate with the Infineon SAK-TC364 MCU(Master mode) and we find that the first few bytes of the data sent by the DSP may not be the preset data in the software.As you can see in the communication timing,the 0xFF52 in the SPI-MISO singnal is a unexpected data.

The figures below are the SPI communication timing and the SPI configuration of the SAK-TC364,could you find any problem from them? And do you have any ideal about this case? Thanks!

111.jpg

image (8).png

  • Hi Liu,

    Apologies for the delay, this thread was just routed to me. Configuration wise, ensure that the clock phase, polarity, CS settings, etc. match on both devices. Have you checked that the controller device is sending the data correctly? If so, have you checked the target device's registers to see if the data is incorrect in SPIDAT, SPIRXBUF, or both. How much data are you transmitting/receiving at a time? Ensure it matches across the devices, and the correct bit-shift is applied when receiving 16 or more bits at a time on the C2000 side. Please work with the controller device's team for questions on the controller. 

    Best Regards,

    Aishwarya

  • Hello Aishwarya,

    We have re-tested this issue over the past few days and observed that when the inter-frame gap between the data sent from the master to the slave is too small (e.g., 320.36μs in this case), the header of the data frame sent by the slave is prone to errors. Specifically, the data in the header of the slave's abnormal frame originates from the tail end of the previous frame sent by the master. After extending the time interval between the two frames sent by the master to 1.3ms, the anomaly did not recur during our re-tests. I am curious whether a small inter-frame gap would affect the slave's data processing? Furthermore, with a baud rate of 1 Mbps, a 320.36μs gap doesn't seem particularly small—why would the data sent by the DSP still encounter anomalies?

    By the way, the Delay time of SPISTE valid to SPICLK is about 580-600ns and the  Delay time of SPICLK to SPISTE invalid is about 80-100ns(as show in the 2 figures below),is there any risk to the DSP SPI work?

  • Liu,

    This is helpful information! HW wise timing requirements seems to be met, but SW wise, it looks like the target application needs some additional time to execute interrupts and process data/prepare any buffers. I would add timing margin to account for this accordingly.

    Best Regards,

    Aishwarya