This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Slow Flash Programming on Uniflash 8.3

Part Number: TMS320F28379D
Other Parts Discussed in Thread: UNIFLASH

Hi,

We are trying to load flash program to the delfino (TMS320F28379D on ti launchpad) using Uniflash 8.3 (we have udpated it to latest one). Uniflash detects the launchpad and starts to load the program but the progress is painfully slow. after waiting for several minutes it has not progressed more than 25%. 
When we try to load the code via CCS debugger goes fast but Uniflash is slow. How can we solve this?
Vinod Ganesh

Decisure Consultancy Services