Hello!
One question about the parameter P in the McBSP timing in master mode.
In data manual (Literature Number: SGUS051A - March 2004 - Revised October 2004) on page 148 the McBSP timing is shown. There the parameter
P is defined as ==> 2P = 1/CLKG, in master mode, too.
Therefore, for example the setup time M49 is 123ns (CLKG = 3,75 MHz = extern clock of the McBSP) and the hold time M50 is 123ns, too.
Is that right? I think there is an error in the calculation. The setup time M49 and the hold time M50 are too much.
What P means exactly?
Yours sincerely, S. Barra