This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P650DK: EtherCAT PDI Watchdog cnt , Process unit error and verify ECATPHYCLK fail

Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: C2000WARE

EtherCAT PDI Watchdog cnt , Process unit error and  verify  ECATPHYCLK fail

 

 

Hi TI Expert:

    I am conducting EtherCAT functional testing on custom hardware. I encountered the following issues:

  1.  I get PDI Watchdog cnt or Process unit error in TwinCAT3
  2. verify  ECATPHYCLK failed

How can i close those issues?

The detailed description is as follows:

  1. my working environment:
    1.  custom hardware based on TMS320F28P650DK7
    2. C2000Ware5.0.0.0
    3. CCS 12.5.0.00007 
    4. TwinCAT3 v3.1.4024.62 (Confirm that the network card and software configuration are good.)
  2. other information:
    1. TwinCAT3 can scan Box but some information incompleted
    2. get error EEPROM size and PDI type in TwinCAT3 Smart View
    3. cant write EEPROM use TwinCAT
    4. get PDI Watchdog cnt or Process unit error in TwinCAT Memory view
    5. verify XTAL freq 25MHz passed
    6. verify SYSCLK freq 200MHz passed
    7. verify ECATPHYCLK freq 100MHz failed, check ECATDIV is 2

Thanks & Regards