Part Number: TMS320F280039C
Dear team,
Fault phenomenon: After downloading the program, F280039C did not run properly when powered on again.
Solution: Configure the F280039C boot option to flash boot through the downloader, then power it back on and F280039C can run normally.
Problem analysis: In the documentation of F280039C, as shown below, if the boot mode is not configured, it will eventually switch to Flash boot.

Because the peripheral hardware circuit of F280039C is not configured with a boot mode, it will be set to flash boot according to the document; But in reality, when we produced more than 500 pcs in this batch, there were 5 abnormal pcs that could not be started normally.
Please help analyze the reasons and whether the meaning expressed in the document we understand is accurate.