Part Number: TMS320F28P550SG
Dear TI Team,
I am building a totem pole PFC system using the TMS320F28P550SG which needs to operate with variable AC frequency. I plan to use the software phase locked loop library functions to help with the control of this system based around one of the TI example designs.
For the TI examples I have seen, all are designed to run with a normal AC frequency of 50 or 60Hz for which the SPLL should work well. However, I need good PLL performance with an AC frequency which varies over a range of approximately 2:1 and am concerned that this maybe compromise PLL performance at the extremes of AC frequency.
Can you provide any guidance on the trade offs I may need to consider with variable frequency operation and what I need to be careful about. The AC frequency will only change frequency quite slowely, of the order of seconds.
Many Thanks,
Iain