This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: Cofigurable logic block using bit field

Part Number: TMS320F280049C

Hey,

I have written my code using the bitfield approach. However, for one complex PWM generation, we need to use the Configurable Logic Block (CLB) to generate EPWM8 from EPWM1 & EPWM4. Unfortunately, I could not find any example codes or clear information online for implementing this using the bitfield approach.

Please let me know how to generate these PWM pulses using CLB.

 

Regards,

Akash

  • Hi Akash,

    Can you explain a little more on what you mean by "generate EPWM8 from EPWM1 & EPWM4". Are you attempting to logically AND the two signals together to create a new third signals (EPWM8)?

    Kind regards,
    AJ Favela 

  • Yes, I am trying to perform a logical AND operation between EPWM1 and EPWM4 to generate EPWM8. I have also attached the image for your reference.

    Regards

    Akash

  • Hi Akash,

    Assuming that you are inputting EPWM1 as input 0 and EPWM4 as input 1, then you should be able to logically AND the two signals by doing the following using bitfields:

    This should allow you to input the two EPWMs into a CLB LUT

    Clb1LogicCfgRegs.CLB_LUT4_IN0.bit.SEL_0 = 24U;  // i0 <- CLB_IN0
    Clb1LogicCfgRegs.CLB_LUT4_IN1.bit.SEL_0 = 25U;  // i1 <- CLB_IN1
    The following will configure the LUT to be used to logically AND the two signals
    Clb1LogicCfgRegs.CLB_LUT4_FN1_0.bit.FN0 = 0x8888U;
    The following will pass the AND'd signal from the LUT and output it via the OUTLUT
    Clb1LogicCfgRegs.CLB_OUTPUT_LUT_0.bit.IN0 = 7U;
    Clb1LogicCfgRegs.CLB_OUTPUT_LUT_0.bit.FN  = 0xAAU;
    Kind regards,
    AJ Favela 
  • Hi AJ

    I have tested the code you provided. Did not get the output. Attaching my code for your reference.

    //#############################################################################
    /
    //
    #include "F28x_Project.h"
    #include "IQmathLib.h"
    #include "math.h"
    //#include "Solar_F.h"
    #include "SFO_V8.h"
    //
    //

    #define PI 3.1459
    float32 TIMER_PERIOD_COUNT=500;
    float32 TIMER_PERIOD_COUNT_ISR=500;
    volatile float Fc=1000, Sw_period=0.00001, Sw_period_isr = 0.00001;
    int deadband=40;
    int deadband_1A=40;
    int deadband_2A=40;
    int tbphs=2;

    #define PWM_CH 3// # of PWM channels + 1

    volatile struct EPWM_REGS *ePWM[PWM_CH] = { &EPwm1Regs, &EPwm1Regs, &EPwm2Regs};
    int MEP_ScaleFactor;
    Uint16 status;


    volatile float v_a, v_pu;
    volatile float radian;
    volatile int k=0;
    Uint32 delay2=0;
    int temp = 0;

    // Function Prototypes

    void Setup_ePWM(void);
    void Gpio_select(void);
    void ConfigureADC(void);
    void SetupADCSoftware(void);
    __interrupt void adcA1ISR(void);
    __interrupt void epwm1_isr(void);
    void error(void);
    //
    // Main
    //
    void main(void)
    {
    //
    //Step 1. Initialize System Control:
    //PLL, WatchDog,enabe Peripheral Clocks
    //This example function is found in the f28004x_sysctrl.c file.
    //
    #ifdef _FLASH
    memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t) &RamfuncsLoadSize);
    #endif
    //
    InitSysCtrl();
    //
    //Step 2. Initialize GPIO
    //
    InitGpio();
    //
    //Step 3. Clear all __interrupts and initialize PIE vector table:
    //Disable CPU __interrupts
    //
    DINT;
    //
    //Initialize the PIE control registers to their default state.
    //The default state is all PIE interrupts disabled and flags
    //are cleared.
    //
    InitPieCtrl();

    //
    //Disable CPU interrupts and clear all CPU interrupt flags:
    //
    IER = 0x0000;
    IFR = 0x0000;

    //
    //Initialize the PIE vector table with pointers to the shell Interrupt
    //Service Routines (ISR).
    //

    InitPieVectTable();
    EALLOW;
    PieVectTable.ADCA1_INT = &adcA1ISR;
    // PieVectTable.EPWM1_INT = &epwm1_isr;
    EDIS;

    EALLOW;
    CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 0;
    EDIS;

    Gpio_select();
    Setup_ePWM();
    ConfigureADC();
    SetupADCSoftware();

    EALLOW;
    CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 1;
    EDIS;
    //////////////////////////

    IER |= M_INT1; // Enable group 1 interrupts (ADC)
    // IER |= M_INT3; // Enable group 3 interrupts (EPWM)

    EINT; // Enable Global interrupt INTM
    ERTM; // Enable Global realtime interrupt DBGM

    // Enable PIE interrupt
    PieCtrlRegs.PIEIER1.bit.INTx1 = 1;
    // PieCtrlRegs.PIEIER3.bit.INTx1 = 1;

    status = SFO_INCOMPLETE;
    while(status == SFO_INCOMPLETE)
    {
    status = SFO();
    if(status == SFO_ERROR)
    {
    error(); // SFO function returns 2 if an error occurs & # of MEP
    } // steps/coarse step exceeds maximum of 255.
    }

    while(1)
    {

    }
    }


    void Setup_ePWM(void)
    {

    EALLOW;
    CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 0;
    EDIS;

    // Setting counter mode and frequency //epwm1 for S5 as well as ADC sampling
    EPwm1Regs.TBCTL.bit.FREE_SOFT = 11;
    EPwm1Regs.TBPRD = TIMER_PERIOD_COUNT;
    EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN;
    EPwm1Regs.TBCTL.bit.CLKDIV = 0;
    EPwm1Regs.TBCTL.bit.HSPCLKDIV = 0;
    EPwm1Regs.TBCTR = 0;

    EPwm1Regs.CMPA.bit.CMPA = 0;
    EPwm1Regs.AQCTLA.bit.CAU = AQ_CLEAR; // Set output low
    EPwm1Regs.AQCTLA.bit.CAD = AQ_SET; // Set output high

    EPwm1Regs.TBCTL.bit.SYNCOSEL =TB_CTR_ZERO;
    EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; //Set as a master
    EPwm1Regs.TBCTL.bit.PHSDIR=TB_UP;

    EPwm1Regs.DBCTL.bit.POLSEL = 2; //Active High Complementary inverted signal will be observed at ePWMB
    EPwm1Regs.DBCTL.bit.OUT_MODE = 3; //fully enabled RED and FED
    EPwm1Regs.DBRED.all = deadband_1A; //RED 200ns
    EPwm1Regs.DBFED.all = deadband_1A; //FED 200ns

    EPwm1Regs.TBCTL.bit.PRDLD= TB_SHADOW; //The period register (TBPRD) is loaded from its shadow register
    EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_PRD; //Load on CTR = Zero: Time-base counter equal to zero
    EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; //Shadow mode

    EPwm1Regs.TBPHS.all = 0;


    /////// ADC SOC generation /////////////

    EPwm1Regs.ETSEL.bit.SOCAEN = 1; //Epwm1A is used as start of conversion for ADC
    EPwm1Regs.ETSEL.bit.SOCASEL = 1; //Enable event time based counter to zero
    EPwm1Regs.ETPS.bit.SOCAPRD = 1; //at every first/third event it has to generate event
    EPwm1Regs.ETCLR.bit.SOCA = 1; //Clear flag

    EPwm1Regs.ETSEL.bit.INTEN = 1; //Enable ePWM Interrupt (EPWMx_INT) Generation
    EPwm1Regs.ETSEL.bit.INTSEL = 1; //enable event time based counter to zero
    EPwm1Regs.ETPS.bit.INTPRD = 1; //at every first/third event it has to generate event
    EPwm1Regs.ETCLR.bit.INT = 1; //Clear flag

    ///////// Epwm2 for S6 ///////////////////
    EPwm2Regs.TBCTL.bit.FREE_SOFT = 11;
    EPwm2Regs.TBPRD = TIMER_PERIOD_COUNT;
    EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN;
    EPwm2Regs.TBCTL.bit.CLKDIV = 0;
    EPwm2Regs.TBCTL.bit.HSPCLKDIV = 0;
    EPwm2Regs.TBCTR = 0;

    EPwm2Regs.CMPA.bit.CMPA = 0;
    EPwm2Regs.AQCTLA.bit.CAU = AQ_CLEAR; // Set output high
    EPwm2Regs.AQCTLA.bit.CAD = AQ_SET; // Set output low

    EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;
    EPwm2Regs.TBCTL.bit.PHSEN = TB_ENABLE; //Set as a master
    EPwm2Regs.TBCTL.bit.PHSDIR=TB_UP;

    EPwm2Regs.DBCTL.bit.POLSEL = 2; //Active High Complementary inverted signal will be observed at ePWMB
    EPwm2Regs.DBCTL.bit.OUT_MODE = 3; //fully enabled RED and FED
    EPwm2Regs.DBRED.all = deadband_2A; //RED 200ns
    EPwm2Regs.DBFED.all = deadband_2A; //FED 200ns

    EPwm2Regs.TBCTL.bit.PRDLD= TB_SHADOW; //The period register (TBPRD) is loaded from its shadow register
    EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_PRD; //Load on CTR = Zero: Time-base counter equal to zero
    EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; //Shadow mode
    EPwm2Regs.TBPHS.bit.TBPHS = 2; //Set phase angle of ePWM1 is 0

    ////////// Epwm3 for hrcap ///////
    EPwm3Regs.TBCTL.bit.FREE_SOFT = 11;
    EPwm3Regs.TBPRD = TIMER_PERIOD_COUNT;
    EPwm3Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN;
    EPwm3Regs.TBCTL.bit.CLKDIV = 0;
    EPwm3Regs.TBCTL.bit.HSPCLKDIV = 0;
    EPwm3Regs.TBCTR = 0;

    EPwm3Regs.CMPA.bit.CMPA = 230;
    EPwm3Regs.AQCTLA.bit.CAU = AQ_CLEAR; // Set output high
    EPwm3Regs.AQCTLA.bit.CAD = AQ_SET; // Set output low

    EPwm3Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;
    EPwm3Regs.TBCTL.bit.PHSEN = TB_ENABLE; //Set as a master
    EPwm3Regs.TBCTL.bit.PHSDIR=TB_UP;

    EPwm3Regs.DBCTL.bit.POLSEL = 2; //Active High Complementary inverted signal will be observed at ePWMB
    EPwm3Regs.DBCTL.bit.OUT_MODE = 3; //fully enabled RED and FED
    EPwm3Regs.DBRED.all = deadband_2A; //RED 200ns
    EPwm3Regs.DBFED.all = deadband_2A; //FED 200ns

    EPwm3Regs.TBCTL.bit.PRDLD= TB_SHADOW; //The period register (TBPRD) is loaded from its shadow register
    EPwm3Regs.CMPCTL.bit.LOADAMODE = CC_CTR_PRD; //Load on CTR = Zero: Time-base counter equal to zero
    EPwm3Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; //Shadow mode
    EPwm3Regs.TBPHS.bit.TBPHS = 2; //Set phase angle of ePWM1 is 0


    ///////////// Epwm4 for S1 ////////

    EPwm4Regs.TBCTL.bit.FREE_SOFT = 11;
    EPwm4Regs.TBPRD = TIMER_PERIOD_COUNT;
    EPwm4Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN;
    EPwm4Regs.TBCTL.bit.CLKDIV = 0;
    EPwm4Regs.TBCTL.bit.HSPCLKDIV = 0;
    EPwm4Regs.TBCTR = 0;

    EPwm4Regs.CMPA.bit.CMPA = 0;
    EPwm4Regs.CMPB.bit.CMPB = 0;
    EPwm4Regs.AQCTLA.bit.CAU = AQ_CLEAR;
    EPwm4Regs.AQCTLA.bit.CBU = AQ_SET;

    EPwm4Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;
    EPwm4Regs.TBCTL.bit.PHSEN = TB_ENABLE; //Set as a master
    EPwm4Regs.TBCTL.bit.PHSDIR=TB_UP;

    EPwm4Regs.DBCTL.bit.POLSEL = 2; //Active High Complementary inverted signal will be observed at ePWMB
    EPwm4Regs.DBCTL.bit.OUT_MODE = 3; //fully enabled RED and FED
    EPwm4Regs.DBRED.all = deadband; //RED 200ns
    EPwm4Regs.DBFED.all = deadband; //FED 200ns

    EPwm4Regs.TBCTL.bit.PRDLD= TB_SHADOW; //The period register (TBPRD) is loaded from its shadow register
    EPwm4Regs.CMPCTL.bit.LOADAMODE = CC_CTR_PRD; //Load on CTR = Zero: Time-base counter equal to zero
    EPwm4Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; //Shadow mode
    EPwm4Regs.TBPHS.bit.TBPHS = 0; //Set phase angle of ePWM1 is 0


    ///////////// Epwm5 for S2 /////////////
    EPwm5Regs.TBCTL.bit.FREE_SOFT = 11;
    EPwm5Regs.TBPRD = TIMER_PERIOD_COUNT;
    EPwm5Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN;
    EPwm5Regs.TBCTL.bit.CLKDIV = 0;
    EPwm5Regs.TBCTL.bit.HSPCLKDIV = 0;
    EPwm5Regs.TBCTR = 0;

    EPwm5Regs.CMPA.bit.CMPA = 0;
    EPwm5Regs.AQCTLA.bit.CAU = AQ_CLEAR; // Set output high
    EPwm5Regs.AQCTLA.bit.CAD = AQ_SET; // Set output low

    EPwm5Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;
    EPwm5Regs.TBCTL.bit.PHSEN = TB_ENABLE; //Set as a master
    EPwm5Regs.TBCTL.bit.PHSDIR=TB_UP;

    EPwm5Regs.DBCTL.bit.POLSEL = 2; //Active High Complementary inverted signal will be observed at ePWMB
    EPwm5Regs.DBCTL.bit.OUT_MODE = 3; //fully enabled RED and FED
    EPwm5Regs.DBRED.all = deadband; //RED 200ns
    EPwm5Regs.DBFED.all = deadband; //FED 200ns

    EPwm5Regs.TBCTL.bit.PRDLD= TB_SHADOW; //The period register (TBPRD) is loaded from its shadow register
    EPwm5Regs.CMPCTL.bit.LOADAMODE = CC_CTR_PRD; //Load on CTR = Zero: Time-base counter equal to zero
    EPwm5Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; //Shadow mode
    EPwm5Regs.TBPHS.bit.TBPHS = 0; //Set phase angle of ePWM1 is 0

    ////////// Epwm6 for S3 ///////////
    EPwm6Regs.TBCTL.bit.FREE_SOFT = 11;
    EPwm6Regs.TBPRD = TIMER_PERIOD_COUNT;
    EPwm6Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN;
    EPwm6Regs.TBCTL.bit.CLKDIV = 0;
    EPwm6Regs.TBCTL.bit.HSPCLKDIV = 0;
    EPwm6Regs.TBCTR = 0;

    EPwm6Regs.CMPA.bit.CMPA = 0;
    EPwm6Regs.AQCTLA.bit.CAU = AQ_CLEAR; // Set output high
    EPwm6Regs.AQCTLA.bit.CAD = AQ_SET; // Set output low

    EPwm6Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;
    EPwm6Regs.TBCTL.bit.PHSEN = TB_ENABLE; //Set as a master
    EPwm6Regs.TBCTL.bit.PHSDIR=TB_UP;

    EPwm6Regs.DBCTL.bit.POLSEL = 2; //Active High Complementary inverted signal will be observed at ePWMB
    EPwm6Regs.DBCTL.bit.OUT_MODE = 3; //fully enabled RED and FED
    EPwm6Regs.DBRED.all = deadband; //RED 200ns
    EPwm6Regs.DBFED.all = deadband; //FED 200ns

    EPwm6Regs.TBCTL.bit.PRDLD= TB_SHADOW; //The period register (TBPRD) is loaded from its shadow register
    EPwm6Regs.CMPCTL.bit.LOADAMODE = CC_CTR_PRD; //Load on CTR = Zero: Time-base counter equal to zero
    EPwm6Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; //Shadow mode

    EPwm6Regs.TBPHS.bit.TBPHS = 0; //Set phase angle of ePWM1 is 0

    ///////// Epwm7 for ADC ////// Only for hybrid modulation program
    EPwm7Regs.TBCTL.bit.FREE_SOFT = 11;
    EPwm7Regs.TBPRD = TIMER_PERIOD_COUNT;
    EPwm7Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN;
    EPwm7Regs.TBCTL.bit.CLKDIV = 0;
    EPwm7Regs.TBCTL.bit.HSPCLKDIV = 0;
    EPwm7Regs.TBCTR = 0;

    EPwm7Regs.CMPA.bit.CMPA = 0;
    EPwm7Regs.AQCTLA.bit.CAU = AQ_CLEAR; // Set output high
    EPwm7Regs.AQCTLA.bit.CAD = AQ_SET; // Set output low

    EPwm7Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;
    EPwm7Regs.TBCTL.bit.PHSEN = TB_ENABLE; //Set as a master
    EPwm7Regs.TBCTL.bit.PHSDIR=TB_UP;

    EPwm7Regs.DBCTL.bit.POLSEL = 2; //Active High Complementary inverted signal will be observed at ePWMB
    EPwm7Regs.DBCTL.bit.OUT_MODE = 3; //fully enabled RED and FED
    EPwm7Regs.DBRED.all = deadband; //RED 200ns
    EPwm7Regs.DBFED.all = deadband; //FED 200ns

    EPwm7Regs.TBCTL.bit.PRDLD= TB_SHADOW; //The period register (TBPRD) is loaded from its shadow register
    EPwm7Regs.CMPCTL.bit.LOADAMODE = CC_CTR_PRD; //Load on CTR = Zero: Time-base counter equal to zero
    EPwm7Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; //Shadow mode

    EPwm7Regs.TBPHS.bit.TBPHS = 0; //Set phase angle of ePWM1 is 0

    ////////// Epwm8 for S4 ///////////

    EPwm8Regs.TBCTL.bit.FREE_SOFT = 11;
    EPwm8Regs.TBPRD = TIMER_PERIOD_COUNT;
    EPwm8Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN;
    EPwm8Regs.TBCTL.bit.CLKDIV = 0;
    EPwm8Regs.TBCTL.bit.HSPCLKDIV = 0;
    EPwm8Regs.TBCTR = 0;


    EPwm8Regs.CMPA.bit.CMPA = 0;
    EPwm8Regs.CMPB.bit.CMPB = 0;
    EPwm8Regs.AQCTLA.bit.CAU = AQ_NO_ACTION;
    EPwm8Regs.AQCTLA.bit.CBU = AQ_NO_ACTION;
    EPwm8Regs.AQCTLA.bit.CAD = AQ_NO_ACTION;
    EPwm8Regs.AQCTLA.bit.CBU = AQ_NO_ACTION;

    EPwm8Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;
    EPwm8Regs.TBCTL.bit.PHSEN = TB_ENABLE; //Set as a master
    EPwm8Regs.TBCTL.bit.PHSDIR=TB_UP;

    EPwm8Regs.DBCTL.bit.POLSEL = 2; //Active High Complementary inverted signal will be observed at ePWMB
    EPwm8Regs.DBCTL.bit.OUT_MODE = 3; //fully enabled RED and FED
    EPwm8Regs.DBRED.all = 0; //RED 200ns
    EPwm8Regs.DBFED.all = 0; //FED 200ns

    EPwm8Regs.TBCTL.bit.PRDLD= TB_SHADOW; //The period register (TBPRD) is loaded from its shadow register
    EPwm8Regs.CMPCTL.bit.LOADAMODE = CC_CTR_PRD; //Load on CTR = Zero: Time-base counter equal to zero
    EPwm8Regs.CMPCTL.bit.SHDWAMODE = CC_IMMEDIATE; //Shadow mode
    EPwm8Regs.CMPCTL.bit.LOADBMODE = CC_CTR_PRD; //Load on CTR = Zero: Time-base counter equal to zero
    EPwm8Regs.CMPCTL.bit.SHDWBMODE = CC_IMMEDIATE; //Shadow mode
    EPwm8Regs.TBPHS.bit.TBPHS = 0; //Set phase angle of ePWM1 is 0

    EALLOW;
    Clb1LogicCfgRegs.CLB_LUT4_IN0.bit.SEL_0 = 24U; // i0 <- CLB_IN0
    Clb1LogicCfgRegs.CLB_LUT4_IN1.bit.SEL_0 = 25U; // i1 <- CLB_IN1
    // The following will configure the LUT to be used to logically AND the two signals
    Clb1LogicCfgRegs.CLB_LUT4_FN1_0.bit.FN0 = 0x8888U;
    // The following will pass the AND'd signal from the LUT and output it via the OUTLUT
    Clb1LogicCfgRegs.CLB_OUTPUT_LUT_0.bit.IN0 = 7U;
    Clb1LogicCfgRegs.CLB_OUTPUT_LUT_0.bit.FN = 0xAAU;

    EDIS;


    // EALLOW;
    // InputXbarRegs.INPUT1SELECT=4;
    // EPwmXbarRegs.TRIP4MUX0TO15CFG.bit.MUX0=0;
    // EPwmXbarRegs.TRIP4MUXENABLE.bit.MUX0 = 1;
    //
    //
    // EPwm8Regs.DCTRIPSEL.bit.DCAHCOMPSEL= 3; // TRIPIN4
    // EPwm8Regs.TZDCSEL.bit.DCAEVT1 = 2; // Digital Compare Output A Event 1 Selection DCAH = high, DCAL = don't care
    // EPwm8Regs.DCACTL.bit.EVT1SRCSEL = 0; // Unfiltered
    // EPwm8Regs.DCACTL.bit.EVT1FRCSYNCSEL = 1; // Asynchronous
    // EPwm8Regs.AQTSRCSEL.bit.T1SEL=0;
    // EPwm8Regs.AQCTLA2.bit.T1D=AQ_SET;
    // EPwm8Regs.AQCTLA2.bit.T1U=AQ_SET;
    // EDIS;

    EALLOW;
    CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 1;
    EDIS;

    }

    void Gpio_select(void)
    {
    EALLOW;

    //setup EPWM PINS
    // Disable internal pull-up for the selected output pins for reduced power
    //epwm1 for S5
    GpioCtrlRegs.GPAPUD.bit.GPIO0 = 1; // Disable pull-up on GPIO0 (EPWM1A)
    GpioCtrlRegs.GPAPUD.bit.GPIO1 = 1; // Disable pull-up on GPIO1 (EPWM1B)
    GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1; // Configure GPIO0 as EPWM1A
    GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 1; // Configure GPIO1 as EPWM1B

    //epwm2 for S6
    GpioCtrlRegs.GPAPUD.bit.GPIO2 = 1; // Disable pull-up on GPIO2 (EPWM2A)
    GpioCtrlRegs.GPAPUD.bit.GPIO3 = 1; // Disable pull-up on GPIO3 (EPWM2B)
    GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 1; // Configure GPIO2 as EPWM2A
    GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 1; // Configure GPIO2 as EPWM2B

    //epwm3 //for hrcap
    GpioCtrlRegs.GPAPUD.bit.GPIO4 = 1; // Disable pull-up on GPIO0 (EPWM3A)
    GpioCtrlRegs.GPAPUD.bit.GPIO5 = 1; // Disable pull-up on GPIO1 (EPWM3B)
    GpioCtrlRegs.GPAMUX1.bit.GPIO4 = 1; // Configure GPIO0 as hrcap
    GpioCtrlRegs.GPAMUX1.bit.GPIO5 = 1; // Configure GPIO2 as hrcap

    //epwm4 for S1
    GpioCtrlRegs.GPAPUD.bit.GPIO6 = 1;
    GpioCtrlRegs.GPAPUD.bit.GPIO7 = 1;
    GpioCtrlRegs.GPAMUX1.bit.GPIO6 = 1;
    GpioCtrlRegs.GPAMUX1.bit.GPIO7 = 1;

    //epwm5 for S2
    GpioCtrlRegs.GPAPUD.bit.GPIO8 = 1; // Disable pull-up on GPIO8 (EPWM5A)
    GpioCtrlRegs.GPAPUD.bit.GPIO9 = 1; // Disable pull-up on GPIO (EPWM5B)
    GpioCtrlRegs.GPAMUX1.bit.GPIO8 = 1; // Configure GPIO8 as EPWM5A
    GpioCtrlRegs.GPAMUX1.bit.GPIO9 = 1;

    //epwm6 for S3
    GpioCtrlRegs.GPAPUD.bit.GPIO10 = 1; // Disable pull-up on GPIO10 (EPWM6A)
    GpioCtrlRegs.GPAPUD.bit.GPIO11 = 1; // Disable pull-up on GPIO1 (EPWM6B)
    GpioCtrlRegs.GPAMUX1.bit.GPIO10 = 1; // Configure GPIO10 as EPWM6A
    GpioCtrlRegs.GPAMUX1.bit.GPIO11 = 1;

    //epwm7 for ADC
    GpioCtrlRegs.GPAPUD.bit.GPIO12 = 1; // Disable pull-up on GPIO10 (EPWM7A)
    GpioCtrlRegs.GPAPUD.bit.GPIO13 = 1; // Disable pull-up on GPIO1 (EPWM7B)
    GpioCtrlRegs.GPAMUX1.bit.GPIO12 = 1; // Configure GPIO10 as EPWM7A
    GpioCtrlRegs.GPAMUX1.bit.GPIO13 = 1;

    //epwm8 for S4
    GpioCtrlRegs.GPAPUD.bit.GPIO14 = 1; // Disable pull-up on GPIO12 (EPWM8A)
    GpioCtrlRegs.GPBPUD.bit.GPIO32 = 1; // Disable pull-up on GPIO (EPWM8B)
    GpioCtrlRegs.GPAMUX1.bit.GPIO14 = 1; // Configure GPIO12 as EPWM8A
    GpioCtrlRegs.GPBMUX1.bit.GPIO32 = 1; // Configure GPIO12 as EPWM8B


    //epwm8 as GPIO
    // GpioCtrlRegs.GPAMUX1.bit.GPIO14 = 0; // Configure GPIO12 as EPWM8A
    // GpioCtrlRegs.GPADIR.bit.GPIO14=1;
    // GpioDataRegs.GPACLEAR.bit.GPIO14=1;
    //
    // GpioCtrlRegs.GPBMUX1.bit.GPIO32 = 0; // Configure GPIO12 as EPWM8B
    // GpioCtrlRegs.GPBDIR.bit.GPIO32 = 1; // Disable pull-up on GPIO (EPWM8B)
    // GpioDataRegs.GPBCLEAR.bit.GPIO32=1;

    //Setting GPIO for Relay operation
    GpioCtrlRegs.GPAMUX1.bit.GPIO15=0; //Setting pin as GPIO for Relay
    GpioCtrlRegs.GPADIR.bit.GPIO15=1; //setting pin as output pin
    GpioDataRegs.GPACLEAR.bit.GPIO15=1; //Clearing the GPIO


    //Setting GPIO for internal time operation
    GpioCtrlRegs.GPAMUX2.bit.GPIO26=0; //Setting pin as GPIO
    GpioCtrlRegs.GPADIR.bit.GPIO26=1; //setting pin as output pin
    GpioDataRegs.GPACLEAR.bit.GPIO26=1; //Clearing the GPIO


    EDIS;
    }

    void ConfigureADC(void)
    {
    // initADC - Function to configure and power up ADCA.
    //
    SetVREF(ADC_ADCA, ADC_INTERNAL, ADC_VREF3P3); // Setup VREF as internal

    EALLOW;
    AdcaRegs.ADCCTL2.bit.PRESCALE = 6; // Set ADCCLK divider to /4
    AdcaRegs.ADCCTL1.bit.INTPULSEPOS = 1; // Set pulse positions to late
    AdcaRegs.ADCCTL1.bit.ADCPWDNZ = 1; // Power up the ADC and then delay for 1 ms
    EDIS;
    DELAY_US(1000);
    }

    void SetupADCSoftware(void)
    {

    EALLOW;
    AdcaRegs.ADCSOC0CTL.bit.CHSEL = 0; // Grid voltage sensor (A0)
    AdcaRegs.ADCSOC0CTL.bit.ACQPS = 9; //sample duration of 10 SYSCLK cycles (100ns/10ns)
    AdcaRegs.ADCSOC0CTL.bit.TRIGSEL = 5; // Trigger on ePWM6 SOCA

    AdcaRegs.ADCSOC1CTL.bit.CHSEL = 1; // Grid current sensor (A1)
    AdcaRegs.ADCSOC1CTL.bit.ACQPS = 9;
    AdcaRegs.ADCSOC1CTL.bit.TRIGSEL = 5;

    // AdcaRegs.ADCSOC3CTL.bit.CHSEL = 3; // Grid current sensor (A3)
    // AdcaRegs.ADCSOC3CTL.bit.ACQPS = 9;
    // AdcaRegs.ADCSOC3CTL.bit.TRIGSEL = 17;

    AdcaRegs.ADCSOC3CTL.bit.CHSEL = 3; // DC current sensor (mid point)
    AdcaRegs.ADCSOC3CTL.bit.ACQPS = 9;
    AdcaRegs.ADCSOC3CTL.bit.TRIGSEL = 5;

    AdcaRegs.ADCSOC4CTL.bit.CHSEL = 4; //DC link voltage sensor (A4)
    AdcaRegs.ADCSOC4CTL.bit.ACQPS = 9;
    AdcaRegs.ADCSOC4CTL.bit.TRIGSEL = 5;

    AdcaRegs.ADCSOC5CTL.bit.CHSEL = 5; // DC current sensor (A5)
    AdcaRegs.ADCSOC5CTL.bit.ACQPS = 9;
    AdcaRegs.ADCSOC5CTL.bit.TRIGSEL = 5;

    AdcaRegs.ADCSOC6CTL.bit.CHSEL = 6; // DC current sensor (A6)
    AdcaRegs.ADCSOC6CTL.bit.ACQPS = 9;
    AdcaRegs.ADCSOC6CTL.bit.TRIGSEL = 5;

    AdcaRegs.ADCINTSEL1N2.bit.INT1SEL = 6; // End of SOC3 will set INT1 flag
    AdcaRegs.ADCINTSEL1N2.bit.INT1E = 1; // Enable INT1 flag
    AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; // Make sure INT1 flag is cleared

    EDIS;

    }

    __interrupt void adcA1ISR(void)
    {


    v_a=250;
    EPwm1Regs.CMPA.bit.CMPA = v_a;

    EPwm2Regs.CMPA.bit.CMPA = v_a;

    EPwm4Regs.DBRED.all = 0;
    EPwm4Regs.CMPA.bit.CMPA = v_a;
    EPwm4Regs.CMPB.bit.CMPB = v_a+deadband;
    EPwm4Regs.AQCTLA.bit.CAU = AQ_CLEAR;
    EPwm4Regs.AQCTLA.bit.CBU = AQ_SET;

    // EPwm8Regs.DBRED.all = 0;
    // EPwm8Regs.DBFED.all = 0;
    // EPwm8Regs.CMPA.bit.CMPA = v_a;
    // EPwm8Regs.CMPB.bit.CMPB = v_a+deadband;
    // EPwm8Regs.CMPC=v_a-deadband;
    // EPwm8Regs.AQCTLA.bit.CAD = AQ_CLEAR;
    // EPwm8Regs.AQCTLA.bit.CAU = AQ_CLEAR;
    // EPwm8Regs.AQCTLA.bit.CBU = AQ_SET;
    // EPwm8Regs.AQCTLA2.bit.T1D=AQ_SET;


    AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //clear INT1 flag
    if(1 == AdcaRegs.ADCINTOVF.bit.ADCINT1)
    {
    AdcaRegs.ADCINTOVFCLR.bit.ADCINT1 = 1; //clear INT1 overflow flag
    AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //clear INT1 flag
    }
    PieCtrlRegs.PIEACK.bit.ACK1 = PIEACK_GROUP1;

    }

    void error (void)
    {
    ESTOP0; // Stop here and handle error
    }

  • Hi Akash,

    The expert is currently out of the office until mid-next week and will get back to you as soon as possible. Thank you for your patience.

    Best Regards,

    Aishwarya

  • Hi Akash,

    I apologize as I was out of the office last week. Thank you for your patience. As I am reading through your code snippet I noticed that you are configuring GPIO's as EPWM's. I assume that you are then attempting to input these GPIO outputs to the CLB to do the logical operations? 

    Kind regards,
    AJ Favela 

  • Hi AJ,

    Thanks for getting back to me.

    To answer your question: Yes, I am using the standard EPWM configuration for EPWM1 and EPWM4, and I want the CLB to receive those internal signals, perform the AND operation, and then drive the EPWM8A output pin with the result. 

    Regards,

    Akash

  • Hi Akash,

    I apologize as my question might not have been clear. Are you attempting to input the GPIO's to the CLB or are you attempting to input specific EPWM's that are generated by the EPWM module on the device?

    Kind regards,
    AJ Favela 

  • Hi AJ,

    I'm attempting to input the specific EPWMs (EPWM 1A and EPWM 4A) that are generated by the EPWM module on the device to CLB and then generate the CLB output based on logic requirements, i.e., logically AND: EPWM 1A and EPWM 4A.

    Regards,

    Akash

  • Hi Akash, 

    Sorry for the late response. 

    It looks like you are not properly setting up the EPWM values to be inputs to the CLB. 

    Please add the following to your code after the setup_ePWM function and before the previous code I provided. 

    // Route EPWM1A to CLB1_IN0
    InputXbarRegs.INPUT1SELECT = 0; // EPWM1A = GPIO0 (mux value 0)
    ClbXbarRegs.AUXSIG0MUX0TO15CFG.bit.MUX1 = 0; // Select INPUT1
    ClbXbarRegs.AUXSIG0MUXENABLE.bit.MUX1 = 1; // Enable MUX1
    // Route EPWM4A to CLB1_IN1
    InputXbarRegs.INPUT2SELECT = 6; // EPWM4A = GPIO6 (mux value 6)
    ClbXbarRegs.AUXSIG1MUX0TO15CFG.bit.MUX2 = 1; // Select INPUT2
    ClbXbarRegs.AUXSIG1MUXENABLE.bit.MUX2 = 1; // Enable MUX2

    Kind regards,

    AJ Favela