This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800133: ADC Conversion

Part Number: TMS320F2800133
Other Parts Discussed in Thread: TMS320F2800132

Dear Sir/Madam,

I want to convert channel A5/GOPI242 of TMS320F2800132 but it is not working 

 

Please check the following code and suggest 

 

// Included Files
//
#include "f28x_project.h"
#include "f280013x_device.h"

#define STAND_ALONE_EPWM
#define CPUTIMER_PERIOD             119999
#define EPWMCLK_MHZ                 60.0

#define EPWM_UPMODE                 1
#define EPWM_UPDOWNMODE             0
#define EPWM_MODESEL                EPWM_UPDOWNMODE

#define TIMER_CONTROL_VARIABLE             
#define MAIN_RELAY_TIME_ms          500 // 500ms   
#define LED_TOGGLE_TIME_ms          1000 // 1 Sec                     
#define DEADBAND_NS                 24      //Dead Band Coming is ~400ns 85      // Dead band Expected --> 500 nSec
#define PERIOD_US                   2999    // 50microSec    //59999--> 1kHz
#define PERIOD_US_UP_DOWN           1500              

/* Commented this Section - 9/11/2025 */
//#define COMP__AU                     150//90      //--> 1.5 microseconds//150     //--> 2.5 microSeconds width lower edge
//#define COMP__BU                     2879//2699//2940    //--> 1 microSeconds//2879    //2699    // --> 2 microseconds width upper edge
//#define COMP__AUD                    1440//90      //--> 1.5 microseconds//150     //--> 2.5 microSeconds width lower edge
//#define COMP__BUD                    60//2699//2940    //--> 1 microSeconds//2879    //2699    // --> 2 microseconds width upper edge

#define TWOMICRO           120  
#define COMP__AU           1370 //(1500-TWOMICRO-DB/2)
#define COMP__BU           1490
#define COMP__BD           1490
#define COMP__AD           1370
#define COMP__A            1370
#define COMP__B            1490
/* New Changes Date- 09/11/2025*/
#if EPWM_MODESEL == EPWM_UPMODE

/*              EPWM Macros that can be tuned                                */
#define db_tuning                   0.5     // Clock Time in micro Seconds
/*                  end                                                     */
#define time_A                      2
#define time_B                      48

#define DEADBAND_DELTA(db_tuning)   ((db_tuning/50)*2999)
#define DEADBAND_NS                 26      //Dead Band Coming is ~400ns 85      // Dead band Expected --> 500 nSec
#define CAL_COM_A(time_A)           ((time_A/50)*PERIOD_US)
#define CAL_COM_B(time_B)           ((time_B/50)*PERIOD_US)
#define COMP__A                     (CAL_COM_A(time_A)+DEADBAND_DELTA(db_tuning))//90+DEADBAND_DELTA(x)//150//90      //--> 1.5 microseconds//150     //--> 2.5 microSeconds width lower edge
#define COMP__B                     (CAL_COM_B(time_B))//2879//2699//2940    //--> 1 microSeconds//2879    //2699    // --> 2 microseconds width upper edge

#endif

#if EPWM_MODESEL == EPWM_UPDOWNMODE

//#define CAL_COM_A(time_A)           ((time_A/50)*PERIOD_US_UP_DOWN)
//#define CAL_COM_B(time_B)           ((time_B/50)*PERIOD_US_UP_DOWN)
//#define COMP__A                     (CAL_COM_A(time_A))//60
//#define COMP__B                     (CAL_COM_A(time_B))//1440

#endif

/* End new Changes             */
#define NTCTemp                     0x00    //  A0  ; 8K-95deg --12k-80deg
#define Vphase                      0x01    //  A1  ;   ADCA channel 1 // R54
#define Vneutral                    0x03    //  A3/C5  ;   ADCA Channel 3 // R40 ??
#define HVDCFBK                     0x06    //  A6  ;   ADCA Channel 6 // R35 ??
#define I_fbk                       0x0F    //  A15 ;   ADCA channel 15 // R50 
#define I_ac                        0x05    //  A5  ;   ADCA Channel 5  // R96

#define ADCgains                    0.005964
#define ADVoltageGain               (553)
#define DCVoltageGain               608.8
#define CrntGain                    0.1
#define XMRGain                     4.28
#define Diodedrop                   3            
#define Rseries                     600000
#define Rx                          3600
#define ADCCounts                   4095

#define RESULTS_BUFFER_SIZE         256

#define GPIO_242_GPIO242                0x01C80400U
#define FRMVER_REV 0X101000
//
// Main
//
unsigned int i                     =     0                   ;
unsigned int relay_state         =     0                   ;
unsigned long int ledBlink        =     0                    ;
volatile unsigned int pwmDelay    =     0                    ;
unsigned int pwmonFlag            =    0                    ;
unsigned int LedD16OnDelay        =    0                    ;
unsigned int f__500ms           =   0                      ;
unsigned int f__100ms           =   0                      ;
unsigned int f__10ms            =   0                      ;
unsigned int f__2ms             =   0                      ;
unsigned int f_LEDToggle        =   0                      ;
unsigned int led_Counter        =   0                      ;

float Source_vin_adc_pin_Vphase                         ;
float Source_vin_adc_pin_Vneutral                       ;
float Source_vin_adc_pin_HVDC                           ;
float Source_vin_adc_pin_I_ac                           ;
float Source_vin_adc_pin_Ifbk                           ;

uint32_t Vphase_Counts                                     ;
uint32_t Vneutral_Counts                                   ;
uint16_t HVDC_Counts                                       ;
uint16_t I_ac_Counts                                       ;
uint16_t I_fbk_Counts                                      ;
uint32_t NTCTemp_Counts                                      ;


int32_t VLine_Counts                                      ;
int32_t VLine_Counts_Rect                                 ;


uint32_t Vphase_value                                    ;
uint32_t ACPhaseV=0;
uint32_t Vphase_adcSum                                   ; 
uint32_t Vneutral_value                                    ; 
uint32_t I_ak_value                                        ; 
uint32_t HVDC_value                                        ; 
uint32_t I_fbk_value                                       ; 

uint32_t adcAResults_Vphase[RESULTS_BUFFER_SIZE]        ;   // Buffer for results
uint32_t adcAResults_Vneutral[RESULTS_BUFFER_SIZE]      ;
uint32_t adcAResults_HVDCFBK[RESULTS_BUFFER_SIZE]       ;
uint32_t adcAResults_I_fbk[RESULTS_BUFFER_SIZE]         ;
uint32_t adcAResults_I_ac[RESULTS_BUFFER_SIZE]          ;

uint32_t VACAdcSum=0;
uint32_t NTCTempSum=0;
uint32_t NTCTempAvg=0;
uint32_t VACSampleCount=0;
uint32_t VAC_AvgVal=0;


uint32_t Vphase_CountsSum=0;
uint32_t Vneutral_CountsSum=0;
uint32_t Vphase_Avg=0;
uint32_t Vphase_AvgVolt=0;
uint32_t VNeutral_Avg=0;
uint32_t VNeutral_AvgVolt=0;

uint16_t index_Vphase ;
uint16_t index_Vneutral ;
uint16_t index_HVDC ;
uint16_t ntcbasedActionFlag=0;
uint16_t ACAbnFlag=0;
unsigned char msg[]="Phase V : XXX";

uint16_t ch1,ch2,ch3,ch4;
uint16_t charAddr=0;
typedef enum
{
    GPIO_ANALOG_DISABLED,       //!< Pin is in digital mode
    GPIO_ANALOG_ENABLED         //!< Pin is in analog mode
} GPIO_AnalogMode;

/*  User Defined API's*/
void Gpio_ePwm(void)                                    ;
void ClockConfig(void)                                  ;
void init_ePWM3(void)                                   ;
void start_ePWM(void)                                   ;
void mainRelay_On(void)                                 ;
void user_Interrupt_Congiguration(void)                 ;
void user_Timer_PeriodSet(void)                         ;

void gpioADC_Mux(void)                                  ;
void initADC(void)                                      ;
void initADCSOC(void)                                   ;
void init_adc_SOC_trigger(void)                         ;
void measurement(void)                                  ;

 


//
// Function Prototypes
//
__interrupt void cpuTimer0ISR(void)                     ;
__interrupt void cpuTimer1ISR(void)                     ;
__interrupt void cpuTimer2ISR(void)                     ;
__interrupt void adcA1ISR(void)                         ;
uint16_t index_I_ac                                     ;   // Index into result buffer
volatile uint16_t bufferFull                            ;   // Flag to indicate buffer is full
uint16_t GPIO33Flag=0;
uint16_t txMsgFlag=0;
uint32_t txdataTimeDelay=0;
void transmitSCIAMessage(unsigned char * msg);
void initSCIAFIFO(void);
void initSCIAEchoback(void);
void main(void)
{
    InitSysCtrl();
    InitGpio();
    EALLOW;
    // LED 1
    GpioCtrlRegs.GPBGMUX1.bit.GPIO32    = 1;
    GpioCtrlRegs.GPBMUX1.bit.GPIO32     = 0;
    GpioCtrlRegs.GPBPUD.bit.GPIO32      = 0;
    GpioCtrlRegs.GPBDIR.bit.GPIO32      = 1; 

    GpioCtrlRegs.GPAGMUX1.bit.GPIO12    = 1;
    GpioCtrlRegs.GPAMUX1.bit.GPIO12     = 0;
    GpioCtrlRegs.GPAPUD.bit.GPIO12      = 0;
    GpioCtrlRegs.GPADIR.bit.GPIO12      = 1; 
    
    // LED 2 
    GpioCtrlRegs.GPBGMUX1.bit.GPIO33    = 1;
    GpioCtrlRegs.GPBMUX1.bit.GPIO33     = 0;
    GpioCtrlRegs.GPBPUD.bit.GPIO33      = 0;
    GpioCtrlRegs.GPBDIR.bit.GPIO33      = 1; 
    EDIS;
    //
    // Initialize PIE and clear PIE registers. Disables CPU interrupts. 
    //
    DINT;
    InitPieCtrl();
    IER = 0x0000;
    IFR = 0x0000;
    //
    // Initialize the PIE vector table with pointers to the shell Interrupt
    // Service Routines (ISR).
    //
    InitPieVectTable();
    
    GpioDataRegs.GPASET.bit.GPIO12      =  1; // Set the bit high
    GpioDataRegs.GPBSET.bit.GPIO33      =  1; // Set the bit high
    
    user_Interrupt_Congiguration()            ; // Configure the CPU Timer 1  Interrupt
    EALLOW;
   // PieVectTable.ADCA1_INT = &adcA1ISR;     // Function for ADCA interrupt 1
    EDIS;
    //
    // Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
    //
    EINT;
    ERTM;

        
    GPIO_SetupPinMux(3, GPIO_MUX_CPU1, 9);
    GPIO_SetupPinOptions(3, GPIO_INPUT, GPIO_PUSHPULL);
    GPIO_SetupPinMux(2, GPIO_MUX_CPU1, 9);
    GPIO_SetupPinOptions(2, GPIO_OUTPUT, GPIO_ASYNC);

    initSCIAFIFO();                         // Initialize the SCI FIFO
    initSCIAEchoback();

    /* Step 1   :   Assigns GPIO 227 Pin 20 DRIVEB --> EPWMB and GPIO 230  Pin 21 DRIVEA --> EPWM B*/
    Gpio_ePwm()             ;
    /* Step 2   :   Configure EPWM Clock, Disable TIME BASE CLOCK for Setting up the Registers*/
    ClockConfig()           ;
    /* Step 3   :   Configure Time- Base , Capture Compare , Action Qualifier Blocks*/
    init_ePWM3()            ;
    /* Step 4   :   Enable Time BASE CLOCk and start the ePWM Module*/
    start_ePWM()            ;

    gpioADC_Mux()           ;

    /* Step 5   :   ADC Power up Sequence                 */
    initADC()               ;
    /* Step 6   :   ADC Channel Configurations            */
    initADCSOC()            ;
    /* Step 7   :   Configure the Event Based SOC Trigger */
    init_adc_SOC_trigger()  ;

    // Enable global Interrupts and higher priority real-time debug events:
    //
    IER |= M_INT1            ;  // Enable group 1 interrupts

    EINT;           // Enable Global interrupt INTM
    ERTM;           // Enable Global realtime interrupt DBGM
    
    /*Enable Pie Interrupts */
   // PieCtrlRegs.PIEIER1.bit.INTx1           = 1;          // ADCA 1 

    /*Initialize the Buffer*/
    for(index_Vphase = 0; index_Vphase < RESULTS_BUFFER_SIZE; index_Vphase++)
    {
        adcAResults_Vphase[index_Vphase]    = 0 ;
        adcAResults_Vneutral[index_Vphase]  = 0 ;
        adcAResults_HVDCFBK[index_Vphase]   = 0 ;
        adcAResults_I_fbk[index_Vphase]     = 0 ;
        adcAResults_I_ac[index_Vphase]      = 0 ;
    }
    index_Vphase    =   0                       ;
    index_Vneutral  =   0                       ;
    index_HVDC      =   0                       ;
    bufferFull      =   0                       ;

    /* Application Step 01 - Switch on the Relay*/
   // GpioDataRegs.GPACLEAR.bit.GPIO12        =  1                      ; // Main Relay off  

    while(1)
    {
        
        ledBlink++;

        if((ntcbasedActionFlag==0)&&(ACAbnFlag==0))
        {
                if(ledBlink<250000)
                {
                    GpioDataRegs.GPBSET.bit.GPIO32      =  1; 
                }
                if(ledBlink>250000)
                {
                 GpioDataRegs.GPBCLEAR.bit.GPIO32    =  1; 

                }
        }

        if(ledBlink>500000)
        {
            ledBlink=0;
            
          

        }
        txdataTimeDelay++;
        if(txdataTimeDelay>=500000)
        {

           // ACPhaseV=241;
             ch1=(Vphase_Avg/100);
             ch2=Vphase_Avg-(ch1*100);
             ch3=ch2/10;
             ch2=ch2%10;

             msg[10]=(ch1)+0x30;
             msg[11]=ch3+0x30;
             msg[12]=ch2+0x30;
             msg[13]='-';
             //Neutral Count
             charAddr=14;
             ch1=(VNeutral_AvgVolt/100);
             ch2=VNeutral_AvgVolt-(ch1*100);
             ch3=ch2/10;
             ch2=ch2%10;

             msg[charAddr++]=(ch1)+0x30;
             msg[charAddr++]=ch3+0x30;
             msg[charAddr++]=ch2+0x30;
            msg[charAddr++]='-';
             //ACPhase
               
              ch1=(ACPhaseV/100);
             ch2=ACPhaseV-(ch1*100);
             ch3=ch2/10;
             ch2=ch2%10;

             msg[charAddr++]=(ch1)+0x30;
             msg[charAddr++]=ch3+0x30;
             msg[charAddr++]=ch2+0x30;

              //ntc count
                        
              
             ch1=(NTCTempAvg/1000);
             ch2=NTCTempAvg-(ch1*1000);
             ch3=ch2/100;
             ch4=ch2-(ch3*100);
             ch2=ch4%10;
             ch4=ch4%10;
             msg[charAddr++]='N';
             msg[charAddr++]=(ch1)+0x30;
             msg[charAddr++]=ch3+0x30;
             msg[charAddr++]=ch2+0x30;
             msg[charAddr++]=ch4+0x30;
            msg[charAddr]=0;

            

            transmitSCIAMessage(msg);
            txdataTimeDelay=0;

        }

        if((pwmDelay>=100)&&(pwmonFlag==0))
        {
             start_ePWM();
            pwmonFlag=1;

        }
        if(pwmDelay>=100)
            pwmDelay=100;

        if((LedD16OnDelay>=500)&&(GPIO33Flag==0))
        {
          //  GpioDataRegs.GPBCLEAR.bit.GPIO33      =  1; 
            GPIO33Flag=1;
        }

        if(LedD16OnDelay>=500)
        {
                LedD16OnDelay=500;

        }

        // while(!bufferFull)
        // {
        // }
        // bufferFull = 0; //clear the buffer full flag

        // if(relay_state == 0)
        // {
        //     mainRelay_On();
        // }

  
     //   measurement();              
        //Temp based action    
        
        if((NTCTempAvg>=3600)   &&(ntcbasedActionFlag==0))
        {
                
                ntcbasedActionFlag=1;

        }
        if((NTCTempAvg<3300)   &&(ntcbasedActionFlag==1))
        {
                
                ntcbasedActionFlag=0;

        }

        if((ACAbnFlag==0)&&(ACPhaseV>=260))
        {

                ACAbnFlag=1;

        }
        if((ACAbnFlag==0)&&(ACPhaseV<160))
        {

               ACAbnFlag=1;

        }
        if((ACAbnFlag==1)&(ACPhaseV>=165)&&(ACPhaseV<=255))
        {

                ACAbnFlag=0;

        }
        if((ACAbnFlag==1)||(ntcbasedActionFlag==1))
        {
                GpioDataRegs.GPBSET.bit.GPIO32      =  1; 
                //PWM ShutDown
        EPwm3Regs.AQCSFRC.bit.CSFA = 1; 
        EPwm3Regs.AQCSFRC.bit.CSFB = 1;

        }
        if((ACAbnFlag==0)&&(ntcbasedActionFlag==0))
        {
                
                
        EPwm3Regs.AQCSFRC.bit.CSFA = 0; 
        EPwm3Regs.AQCSFRC.bit.CSFB = 0;

        }

 

      


    }

}

/*GPIO Muxing Channels*/
void Gpio_ePwm(void)
{
    EALLOW;
    /*GPIO Muxing*/
    GpioCtrlRegs.GPHMUX1.bit.GPIO227    = 3;   
    GpioCtrlRegs.GPHMUX1.bit.GPIO230    = 3;

    GpioCtrlRegs.GPHDIR.bit.GPIO227     = 1;   // output
    GpioCtrlRegs.GPHDIR.bit.GPIO230     = 1;   // output

    GpioCtrlRegs.GPHPUD.bit.GPIO227     = 1;   // Enable internal pull-up (0=enabled, 1=disabled)
    GpioCtrlRegs.GPHQSEL1.bit.GPIO227   = 0;   // Qualification = sync to sysclk

    GpioCtrlRegs.GPHPUD.bit.GPIO230     = 1;   // Enable internal pull-up (0=enabled, 1=disabled)
    GpioCtrlRegs.GPHQSEL1.bit.GPIO230   = 0;   // Qualification = sync to sysclk
    EDIS;
}

/* ePWM Clock initialization*/
void ClockConfig(void)
{

    /*
        The TBCLKSYNC bit in the peripheral clock enable registers allows all users to globally synchronize all enabled
        ePWM modules to the time-base clock (TBCLK). When set, all enabled ePWM module clocks are started with
        the first rising edge of TBCLK aligned. For synchronized TBCLKs, the prescalers for each ePWM module must
        be set identically.
        The proper procedure for enabling ePWM clocks is as follows:
        1. Enable ePWM module clocks in the PCLKCRx register
        2. Set TBCLKSYNC= 0
        3. Configure ePWM modules
        4. Set TBCLKSYNC= 1
    */
    EALLOW;
    CpuSysRegs.PCLKCR2.bit.EPWM3        = 1; // Enable EPWM3 Clock  
    CpuSysRegs.PCLKCR0.bit.TBCLKSYNC    = 0; // Disable Time Base Clock
    EDIS;
}

void start_ePWM(void)
{
    EALLOW;

    CpuSysRegs.PCLKCR0.bit.TBCLKSYNC    = 1;    // Disable Time Base Clock
    EDIS;
}

/* ePWM 3 Configurations for TB , AQ and CC block */

void init_ePWM3(void)
{
    #if EPWM_MODESEL== EPWM_UPMODE

    // Time Base Block Congigurations
    EPwm3Regs.TBPRD                     = PERIOD_US             ;   // Period register → sets freq
    EPwm3Regs.TBCTL.bit.CTRMODE         = 0                     ;   // Up count mode

    // Duty Set EPWM3A and EPWM3B
    EPwm3Regs.CMPA.bit.CMPA             = COMP__A               ;    
    EPwm3Regs.CMPB.bit.CMPB             = COMP__B               ;     
    // Set the Phase sections
    EPwm3Regs.TBPHS.bit.TBPHS           = 0                     ;   // Set as master ; Phase = 0 
    EPwm3Regs.TBCTR                     = 0                     ;   // Set Time Base counter to 0

    EPwm3Regs.TBCTL.bit.HSPCLKDIV       = 1                     ;   // Clock divide = /2
    EPwm3Regs.TBCTL.bit.CLKDIV          = 0                     ;   // Clock divide = /1

    #ifdef STAND_ALONE_EPWM
    EPwm3Regs.EPWMSYNCINSEL.bit.SEL     = 0                     ;   // Disable Sychronizations
    EPwm3Regs.TBCTL.bit.PHSEN           = 0                     ;   // Disable phase loading
    #endif

    // Counter Compare Block Configurations

    EPwm3Regs.CMPCTL.bit.SHDWAMODE      = 0                     ;   // Double Buffer via CPU Shadow Register
    EPwm3Regs.CMPCTL.bit.SHDWBMODE      = 0                     ;   // Double Buffer via CPU Shadow Register
    EPwm3Regs.CMPCTL.bit.LOADAMODE      = 0                     ;   // Load to Active Register when CTR = 0
    EPwm3Regs.CMPCTL.bit.LOADBMODE      = 0                     ;   // Load to Active Register when CTR = 0
    
    // Action Qualifiers Block Configurations
    EPwm3Regs.AQCTLA.all                =   0                   ;
    EPwm3Regs.AQCTLB.all                =   0                   ;

    EPwm3Regs.AQCTLA.bit.CAU            =   1                   ;   // Clear EPWM 3A When CTR = CMPA while Up Count.
    EPwm3Regs.AQCTLA.bit.ZRO            =   2                   ;   // Set High EPWM 3A when CTR = 0 .Clear EPWM 3B when CTR = Period .

    EPwm3Regs.AQCTLB.bit.CBU            =   2                   ;   // Set High EPWM 3B When CTR = CMPA while Up Count.
    EPwm3Regs.AQCTLB.bit.PRD            =   1                   ;   // Set High EPWM 3B when CTR = 0 .

    /* Dead Band Configuration */

    EPwm3Regs.DBCTL.bit.IN_MODE         =   DBA_ALL             ;   // 0x00 --> EPWMA is the source for both the delays. 
    EPwm3Regs.DBCTL.bit.OUT_MODE        =   DBA_ENABLE          ;   // 0x2--> Enable Dead band for EPWM3A.

    EPwm3Regs.DBCTL.bit.POLSEL          =   DB_ACTV_HI          ;   // 0x0 --> No Complementry .
    EPwm3Regs.DBRED.all                 =   DEADBAND_NS         ;   // [Number of Ticks = TBCLK/Deadband Time] 
    EPwm3Regs.DBFED.all                 =   DEADBAND_NS         ;
    /* Shadow behavior: keep shadows enabled or disabled per your design. We used load on CTR=0 above. */
    #endif

    #if EPWM_MODESEL == EPWM_UPDOWNMODE
        // Time Base Block Congigurations
    EPwm3Regs.TBPRD                 = PERIOD_US_UP_DOWN     ;   // Period register → sets freq
    EPwm3Regs.TBCTL.bit.CTRMODE     = 2                     ;   // Up-Down count mode
    
    EPwm3Regs.TBCTL.bit.HSPCLKDIV   = 1                     ;   // Clock divide = /2
    EPwm3Regs.TBCTL.bit.CLKDIV      = 0                     ;   // Clock divide = /1

    #ifdef STAND_ALONE_EPWM
    EPwm3Regs.EPWMSYNCINSEL.bit.SEL = 0                     ;   // Disable Sychronizations
    EPwm3Regs.TBCTL.bit.PHSEN       = 0                     ;   // Disable phase loading

    #endif

    // Counter Compare Block Configurations

    EPwm3Regs.CMPCTL.bit.SHDWAMODE  = 0                     ;   // Double Buffer via CPU Shadow Register
    EPwm3Regs.CMPCTL.bit.SHDWBMODE  = 0                     ;   // Double Buffer via CPU Shadow Register
    EPwm3Regs.CMPCTL.bit.LOADAMODE  = 0                     ;   // Load to Active Register when CTR = 0
    EPwm3Regs.CMPCTL.bit.LOADBMODE  = 0                     ;   // Load to Active Register when CTR = 0
    
    // Action Qualifiers Block Configurations

    EPwm3Regs.CMPA.bit.CMPA         = COMP__A  ;    // 50% duty for A
    EPwm3Regs.CMPB.bit.CMPB         = COMP__B    ;    // 25% duty for B

    EPwm3Regs.AQCTLA.bit.CAU        = 2                     ;   // Set High EPWM 3A When CTR = CMPA while Up Count.
    EPwm3Regs.AQCTLA.bit.CAD        = 0                     ;   // Clear EPWM 3A When CTR = CMPA while Down Count.
    EPwm3Regs.AQCTLA.bit.CBU        = 1                     ;
    EPwm3Regs.AQCTLA.bit.CBD        = 0                     ;


    EPwm3Regs.AQCTLB.bit.CAU        = 0                     ;   // Clear EPWM 3B When CTR = CMPB while Up Count.
    EPwm3Regs.AQCTLB.bit.CBU        = 0                     ;   // Set High EPWM 3B When CTR = CMPB while Down Count.   
    EPwm3Regs.AQCTLB.bit.CBD        = 2                     ; 
    EPwm3Regs.AQCTLB.bit.CAD        = 1                     ; 
    // Set the Compare Values (Duty Cycle)
   
    


    #endif
}

void user_Interrupt_Congiguration(void)
{

    // Map ISR functions
    //
    EALLOW;

    PieVectTable.TIMER0_INT = &cpuTimer0ISR;

    EDIS;

    // Initialize the Device Peripheral. For this example, only initialize the
    // Cpu Timers.

    InitCpuTimers();

    // Configure CPU-Timer 0, 1, and 2 to interrupt every second:
    // 100MHz CPU Freq, 1 second Period (in uSeconds)

    //ConfigCpuTimer(&CpuTimer0, 100, 1000);
    ConfigCpuTimer(&CpuTimer0, 120, 10);
    //ConfigCpuTimer(&CpuTimer2, 100, 1000);

    //
    // To ensure precise timing, use write-only instructions to write to the
    // entire register. Therefore, if any of the configuration bits are changed
    // in ConfigCpuTimer and InitCpuTimers, the below settings must also be
    // be updated.

    CpuTimer0Regs.TCR.all = 0x4000;
 

    //
    // Enable CPU int1 which is connected to CPU-Timer 0, CPU int13
    // which is connected to CPU-Timer 1, and CPU int 14, which is connected
    // to CPU-Timer 2
    //
    IER |= M_INT1;
   // IER |= M_INT13;
    //IER |= M_INT14;
    //
    // Enable TINT0 in the PIE: Group 1 interrupt 7
    //
    PieCtrlRegs.PIEIER1.bit.INTx7 = 1;
    }

// For Timer 0 
void user_Timer_PeriodSet(void)
{
    //Timer->RegsAddr->PRD.all = temp - 1;
    CpuTimer0Regs.PRD.all   = CPUTIMER_PERIOD;
    //
    // Set pre-scale counter to divide by 1 (SYSCLKOUT)
    //
    CpuTimer0Regs.TPR.all       =   0;
    CpuTimer0Regs.TPRH.all      =   0;

    CpuTimer0Regs.TCR.bit.TSS      =   1;
    //
    // 1 = reload timer
    //
    CpuTimer0Regs.TCR.bit.TRB       =   1;
    CpuTimer0Regs.TCR.bit.SOFT      =   1;

    CpuTimer0Regs.TCR.bit.FREE      =   0;

    CpuTimer0Regs.TCR.bit.TIE      =   1;

}

/*Function to Switch on the Relay after 2 Seconds after power on*/
void mainRelay_On(void)
{
        if(f__500ms == 1 )
        {
            relay_state                         =   1   ;  
            GpioDataRegs.GPASET.bit.GPIO12      =   1   ;   // Main Relay on
        }        
}


/*initADC - Function to configure and power up ADCA.*/

void initADC(void)
{
    //
    // Setup VREF as internal
    //
    SetVREF(ADC_ADCA, ADC_INTERNAL, ADC_VREF3P3);

    EALLOW;
    //
    // Set ADCCLK divider to /4
    //
    AdcaRegs.ADCCTL2.bit.PRESCALE = 6;

    //
    // Set pulse positions to late
    //
    AdcaRegs.ADCCTL1.bit.INTPULSEPOS = 1;

    //
    // Power up the ADC and then delay for 1 ms
    //
    AdcaRegs.ADCCTL1.bit.ADCPWDNZ = 1;
    EDIS;

    DELAY_US(1000);
}

/*Function to configure ADCA's SOC0 to be triggered by ePWM3.*/
void initADCSOC(void)
{
    //
    // Select the channels to convert and the end of conversion flag
    //
    EALLOW;
   
    // 0:A0  1:A1  2:A2  3:A3
    // 4:A4   5:A5   6:A6   7:A7
    // 8:A8   9:A9   A:A10  B:A11
    // C:A12  D:A13  E:A14  F:A15
    AdcaRegs.ADCSOC7CTL.bit.CHSEL           = Vphase            ;

    AdcaRegs.ADCSOC8CTL.bit.CHSEL           = Vneutral          ;//Vneutral

    AdcaRegs.ADCSOC9CTL.bit.CHSEL           = NTCTemp           ;//HVDCFBK

    AdcaRegs.ADCSOC10CTL.bit.CHSEL           = I_fbk            ;
    AdcaRegs.ADCSOC11CTL.bit.CHSEL           = I_ac             ;

    /*Burst Mode Configuration- SOC0, SOC1 , SOC 2 and SOC 3*/

    AdcaRegs.ADCBURSTCTL.bit.BURSTEN        =   1           ;// Enable Burst Mode 
    AdcaRegs.ADCBURSTCTL.bit.BURSTSIZE      =   4          ;// 5 SOC's are converted in One Time 
    AdcaRegs.ADCBURSTCTL.bit.BURSTTRIGSEL   =   9           ;//09h BURSTTRIG9 - ePWM3, ADCSOCA
    AdcaRegs.ADCSOCPRICTL.bit.SOCPRIORITY   =   0xC           ;//Setting burst enabled from SOC0 to SOC11

    AdcaRegs.ADCSOC7CTL.bit.ACQPS           =   10           ;// Sample window is 10 SYSCLK cycles
    AdcaRegs.ADCSOC8CTL.bit.ACQPS           =   10           ;// Sample window is 10 SYSCLK cycles
    AdcaRegs.ADCSOC9CTL.bit.ACQPS           =   10           ;// Sample window is 10 SYSCLK cycles
    AdcaRegs.ADCSOC10CTL.bit.ACQPS           =  10           ;// Sample window is 10 SYSCLK cycles
    AdcaRegs.ADCSOC11CTL.bit.ACQPS           =  10           ; 

    AdcaRegs.ADCSOC7CTL.bit.TRIGSEL         =   0           ;// 09h ADCTRIG9 - ePWM3, ADCSOCA
    AdcaRegs.ADCSOC8CTL.bit.TRIGSEL         =   0           ;// 09h ADCTRIG9 - ePWM3, ADCSOCA
    AdcaRegs.ADCSOC9CTL.bit.TRIGSEL         =   0           ;// 09h ADCTRIG9 - ePWM3, ADCSOCA
    AdcaRegs.ADCSOC10CTL.bit.TRIGSEL         =  0           ;// 09h ADCTRIG9 - ePWM3, ADCSOCA
    AdcaRegs.ADCSOC11CTL.bit.TRIGSEL         =  0           ;

    AdcaRegs.ADCINTSEL1N2.bit.INT1E         =   1             ;// Enable INT1 flag
    AdcaRegs.ADCINTSEL1N2.bit.INT1SEL       =   0xB             ;// End of EOC11 will set INT1 flag
    
    AdcaRegs.ADCINTFLGCLR.bit.ADCINT1       =   1             ;// Make sure INT1 flag is cleared

    EDIS;
}

/*Function to configure ePWM1 to generate the SOC.*/
void init_adc_SOC_trigger(void)
{
    EALLOW;

    EPwm3Regs.ETSEL.bit.SOCAEN  = 1;        // Enable SOC on A group
    EPwm3Regs.ETSEL.bit.SOCASEL = 1;        // Select SOC on up-count CMP B 
    EPwm3Regs.ETPS.bit.SOCAPRD  = 1;         // Generate pulse on 1st event
    EDIS;
}

/*adcA1ISR - ADC A Interrupt 1 ISR*/

__interrupt void adcA1ISR(void)
{
    //
    // Add the latest result to the buffer
    // ADCRESULT0 is the result register of SOC0
    adcAResults_Vphase[index_Vphase++]      = AdcaResultRegs.ADCRESULT0;
    adcAResults_Vneutral[index_Vneutral++]  = AdcaResultRegs.ADCRESULT1;
    adcAResults_HVDCFBK[index_HVDC++]       = AdcaResultRegs.ADCRESULT2;
    adcAResults_I_fbk[index_Vphase++]       = AdcaResultRegs.ADCRESULT3;
    adcAResults_I_ac[index_Vphase++]        = AdcaResultRegs.ADCRESULT4;
    //
    // Set the bufferFull flag if the buffer is full
    //
    if(RESULTS_BUFFER_SIZE <= index_Vphase)
    {
        index_Vphase    = 0;
        index_Vneutral  = 0;
        index_HVDC      = 0;
        bufferFull      = 1;
    }

    //
    // Clear the interrupt flag
    //
    AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1;

    //
    // Check if overflow has occurred
    //
    if(1 == AdcaRegs.ADCINTOVF.bit.ADCINT1)
    {
        AdcaRegs.ADCINTOVFCLR.bit.ADCINT1 = 1; //clear INT1 overflow flag
        AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //clear INT1 flag
    }

    //
    // Acknowledge the interrupt
    //
    PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
}
/*Measurement - ADC Channels */
void measurement(void)
{
        Vphase_Counts                       = (AdcaResultRegs.ADCRESULT7)   ;
        Vneutral_Counts                     = (AdcaResultRegs.ADCRESULT8)   ;
      //  HVDC_Counts                         = (AdcaResultRegs.ADCRESULT9)   ;
        NTCTemp_Counts                      = (AdcaResultRegs.ADCRESULT9)   ;
        I_ac_Counts                         = (AdcaResultRegs.ADCRESULT10)  ;
        I_fbk_Counts                        = (AdcaResultRegs.ADCRESULT11)  ;
        VLine_Counts = Vphase_Counts-Vneutral_Counts;
        if(VLine_Counts < 0)
            VLine_Counts_Rect = -VLine_Counts;
        else
            VLine_Counts_Rect = VLine_Counts;
        VACAdcSum=VACAdcSum+VLine_Counts_Rect;
        NTCTempSum = NTCTempSum + NTCTemp_Counts;

        Vphase_CountsSum=Vphase_CountsSum+Vphase_Counts;
        Vneutral_CountsSum=Vneutral_CountsSum+Vneutral_Counts;

        VACSampleCount++;
        if(VACSampleCount>=10000)
        {
                Vphase_Avg = Vphase_CountsSum/VACSampleCount;
                Vphase_AvgVolt = (ADVoltageGain*Vphase_Avg);
                Vphase_AvgVolt = Vphase_AvgVolt/4096;
                VNeutral_Avg = Vneutral_CountsSum/VACSampleCount;
                VNeutral_AvgVolt = (ADVoltageGain*VNeutral_Avg);
                VNeutral_AvgVolt = VNeutral_AvgVolt/4096;
                


                VAC_AvgVal=VACAdcSum/VACSampleCount;
                Vphase_value=(ADVoltageGain*VAC_AvgVal);
                Vphase_value = Vphase_value/4096;
                ACPhaseV=1.11*Vphase_value;
                ACPhaseV=ACPhaseV+Diodedrop;
                NTCTempAvg = NTCTempSum/VACSampleCount;
                VACSampleCount=0;
                VACAdcSum=0;
                NTCTempSum=0;
                Vneutral_CountsSum=0;
                Vphase_CountsSum=0;

        }

}


void gpioADC_Mux(void)
{
    EALLOW;
    // GPIO analog Mode selection 

    // Vneutral
    GpioCtrlRegs.GPHAMSEL.bit.GPIO242       =   1                                           ; // Enable the analog mode 
    // HVDC
    GpioCtrlRegs.GPHAMSEL.bit.GPIO228       =   1                                           ; // Enable the analog mode 

    EDIS;
}

//
// cpuTimer1ISR - CPU Timer1 ISR with interrupt counter
//
__interrupt void cpuTimer0ISR(void)
{
    //
    // The CPU acknowledges the interrupt
    //
    CpuTimer1.InterruptCount++;
    led_Counter++;
    pwmDelay++;
    LedD16OnDelay++;
    
    if(relay_state == 0) // check the flag setting condition
    {
        if(CpuTimer1.InterruptCount == MAIN_RELAY_TIME_ms)
        {
            f__500ms =   1   ; // Set the timeer flag
        }
    }

    if(led_Counter == LED_TOGGLE_TIME_ms)
    {
        f_LEDToggle                             =   1       ;
        led_Counter                             =   0       ;
       GpioDataRegs.GPBTOGGLE.bit.GPIO33      =   1       ; 
    }else 
    {
        f_LEDToggle =   0   ;
    }
    measurement();  
    AdcaRegs.ADCSOCFRC1.all=0x07FF;
    PieCtrlRegs.PIEACK.all=PIEACK_GROUP1;

 #if 0
95deg                80deg
3.3                3.3
8000                12000
100000                100000
                
3.055555556                2.946428571
3792.592593                3657.142857
#endif

}

//
// End of File
//
void initSCIAEchoback(void)
{
    //
    // Note: Clocks were turned on to the SCIA peripheral
    // in the InitSysCtrl() function
    //
    SciaRegs.SCICCR.all = 0x0007;           // 1 stop bit,  No loopback
                                            // No parity, 8 char bits,
                                            // async mode, idle-line protocol
    SciaRegs.SCICTL2.all = 0x0003;          // enable TX, RX, internal SCICLK,
                                            // Disable RX ERR, SLEEP, TXWAKE

    SciaRegs.SCICTL1.bit.RXENA=1;
    SciaRegs.SCICTL1.bit.TXENA=1;
    SciaRegs.SCICTL2.all = 0x0003;
    SciaRegs.SCICTL2.bit.TXINTENA = 1;
    SciaRegs.SCICTL2.bit.RXBKINTENA = 1;

    //
    // SCIA at 19200 baud
    // @LSPCLK = 25 MHz (100 MHz SYSCLK) HBAUD = 0x01  and LBAUD = 0x44.
    //
    SciaRegs.SCIHBAUD.all = 0x000;
    SciaRegs.SCILBAUD.all = 0x00C2;

    SciaRegs.SCICTL1.all = 0x0023;          // Relinquish SCI from Reset
}

void transmitSCIAChar(uint16_t a)
{
    while (SciaRegs.SCIFFTX.bit.TXFFST != 0)
    {

    }
    SciaRegs.SCITXBUF.all = a;
}

//
// transmitSCIAMessage - Transmit message via SCIA
//
void transmitSCIAMessage(unsigned char * msg)
{
    int i;
    i = 0;
    while(msg[i] != '\0')
    {
        transmitSCIAChar(msg[i]);
        i++;
    }
}

//
// initSCIAFIFO - Initialize the SCI FIFO
//
void initSCIAFIFO(void)
{
    SciaRegs.SCIFFTX.all = 0xE040;
    SciaRegs.SCIFFRX.all = 0x2044;
    SciaRegs.SCIFFCT.all = 0x0;
}

  • Hi Ramesh,

    GPIO242 corresponds to ADC channels A3/C5, not A5 [1][2]. Your code correctly selects channel A5 (I_ac = 0x05) in the SOC configuration, but then enables analog mode on GPIO242—which is a completely different ADC input. This mismatch means the physical pin you're configuring isn't connected to the channel you're trying to sample.

    According to the device pinout, ADC channel A5 is mapped to AIO244 (depending on package variant), not GPIO242 [2][3]. Make a change at the below line of code to enable AIO244.
    // Current code - 
    GpioCtrlRegs.GPHAMSEL.bit.GPIO242 = 1; // change to GPIO244
    Thanks
    Srikanth
  • Thanks Srikant,

    I have issue of ADC Conversion of Channel A3/C5/GPIO242. Kindly check again and share your feedback.

  • Hi Ramesh,

    Your code has four distinct bugs preventing A5/GPIO242 from converting correctly. Here they are in order of severity.

    Bug 1 (Critical): GPIO242 is Channel A3, Not A5

    This is the root hardware mismatch. On the TMS320F2800132 48-pin PT package, GPIO242 (pin 5) is multiplexed with ADCA channel A3 and ADCC channel C5 — not A5 [1][2]. Channel A5 physically lives on GPIO244 (AIO244) on a different pin entirely [2].

    Your gpioADC_Mux() correctly enables analog mode on GPIO242, but initADCSOC() then tells SOC11 to sample channel A5 (CHSEL = 0x05). The ADC is sampling a pin that has no signal on it.

    Pin-to-channel mapping for reference:

    GPIO
    ADC Channel
    Package Pin
    GPIO242
    A3 / C5
    Pin 5
    GPIO244
    A5
    Different pin

    Fix — choose one option:

    Option A — Keep using GPIO242, change the channel selector to A3:
    // In initADCSOC()
    AdcaRegs.ADCSOC11CTL.bit.CHSEL = 0x03; // A3 matches GPIO242
    // Also update the macro definition at the top:
    #define I_ac 0x03 // A3/C5 ; GPIO242
    Option B — Keep using channel A5, switch to the correct GPIO pin:
    // In gpioADC_Mux() — replace GPIO242 with GPIO244
    GpioCtrlRegs.GPHAMSEL.bit.GPIO244 = 1; // Enable analog mode for A5
    // Keep CHSEL = 0x05 (A5) as-is
    Verify your PCB schematic to confirm which physical pin your I_ac signal is routed to before choosing [1][2].
    Bug 2 (Critical): Software Force Overrides the ePWM Trigger

    Inside cpuTimer0ISR(), this line fires every 10 µs:

    AdcaRegs.ADCSOCFRC1.all = 0x07FF; // Forces SOC0–SOC10 only

    The bitmask 0x07FF covers bits 0–10, which does not include SOC11 (the I_ac channel) [3][4]. This means:

    • SOC11 never gets a software trigger from this line
    • The software force conflicts with your burst mode ePWM3 trigger configuration, causing unpredictable sequencing

    Fix: Remove this line entirely and rely on the ePWM3 hardware trigger as intended. If you need a software fallback, use 0x0F80 to force only SOC7–SOC11:

    // Remove this:
    // AdcaRegs.ADCSOCFRC1.all = 0x07FF;
    // If software trigger is needed for debug only:
    // AdcaRegs.ADCSOCFRC1.all = 0x0F80; // SOC7–SOC11
    Bug 3 (Critical): SOC TRIGSEL Must Match Burst Trigger

    All five SOC trigger selectors are set to 0 (software-only trigger):

    AdcaRegs.ADCSOC7CTL.bit.TRIGSEL = 0; // Wrong — disables hardware trigger
    AdcaRegs.ADCSOC8CTL.bit.TRIGSEL = 0;
    // ... same for SOC9, SOC10, SOC11
    In burst mode, the first SOC in the burst sequence must have its TRIGSEL set to match the burst trigger source [3]. With BURSTTRIGSEL = 9 (ePWM3 ADCSOCA), SOC7's TRIGSEL must also be 9. Without this, the burst never fires from the hardware event.

    Fix:

    AdcaRegs.ADCSOC7CTL.bit.TRIGSEL = 9; // ePWM3 ADCSOCA — must match BURSTTRIGSEL
    AdcaRegs.ADCSOC8CTL.bit.TRIGSEL = 0; // Remaining SOCs in burst: leave at 0
    AdcaRegs.ADCSOC9CTL.bit.TRIGSEL = 0;
    AdcaRegs.ADCSOC10CTL.bit.TRIGSEL = 0;
    AdcaRegs.ADCSOC11CTL.bit.TRIGSEL = 0;
    Bug 4 (Moderate): Result Register Swap in measurement()

    Your SOC-to-channel assignments are:

    • SOC10 → I_fbk (channel A15)
    • SOC11 → I_ac (channel A5/A3)

    Each SOCx stores its result in ADCRESULTx — a direct one-to-one mapping [4]. But measurement() reads them backwards:

    // Current code — WRONG assignment:
    I_ac_Counts = (AdcaResultRegs.ADCRESULT10); // This is actually I_fbk data
    I_fbk_Counts = (AdcaResultRegs.ADCRESULT11); // This is actually I_ac data

    Fix — swap the two lines:

    I_fbk_Counts = (AdcaResultRegs.ADCRESULT10); // SOC10 = I_fbk (A15)
    I_ac_Counts = (AdcaResultRegs.ADCRESULT11); // SOC11 = I_ac (A3 or A5)

    Summary of All Fixes

    #
    Location
    Problem
    Fix
    1
    gpioADC_Mux() / initADCSOC()
    GPIO242 = A3, not A5
    Change CHSEL to 0x03, or switch to GPIO244
    2
    cpuTimer0ISR()
    ADCSOCFRC1 = 0x07FF conflicts with burst, misses SOC11
    Remove the line
    3
    initADCSOC()
    All TRIGSEL = 0 prevents ePWM3 from firing burst
    Set SOC7CTL.TRIGSEL = 9
    4
    measurement()
    ADCRESULT10/11 assigned to wrong variables
    Swap I_ac_Counts and I_fbk_Counts

    Additional Notes

    • Hardware startup risk: If your I_ac signal comes from a high-impedance voltage divider, connect it through an RC filter (e.g., 100Ω + 10nF) before the ADC pin. Direct high-impedance connections to ADC inputs on this device have been reported to cause startup failures [5].
    • adcA1ISR is commented out in the PIE vector table and PIE enable register. The ISR also reads ADCRESULT0–4 which don't contain your SOC7–11 data. Since measurement() is called from the timer ISR instead, this is fine — but leave the ISR disabled or update it to read ADCRESULT7–11 if you re-enable it [4].
    • SOCPRIORITY = 0xC sets SOC0–SOC11 in round-robin, which is correct for burst starting at SOC7 [3].

    Citation Index

    1. TMS320F2800132 Device-Specific Pin Map (SPRUJE9)
    2. TMS320F2800132 Datasheet — Pin Attributes Table (SPRSP63B)
    3. C2000 ADC Academy — Burst Mode & SOC Trigger Configuration
    4. TMS320F2800132 Technical Reference Manual — ADC Result Registers (SPRUIN7C)
    5. TI E2E Forum — ADC Input on Pin 5 (A3/C5/GPIO242) Startup Issue