Part Number: F29H85X-SOM-EVM
We have develped a project to operate on a F29H85-SOM-EVM that will eventually run on a custom board. We are currently experiencing NMI issues. When launching via the CCS debugger the board runs as expeted. However if we reset the board or start the board without the debugger it does not run. It would seem that it experiences a NMI and stops. Hoping this is a simple code bug which I just cannot currently see. I would like to understand how I can investigate the source and reason for this NMI. Can you please point me to some documentation that would help me understand what is going on?