Part Number: TMS320F2800157-Q1
Other Parts Discussed in Thread: POWERSUITE
Hi expert,
Customer has questions about pmp23340 scaling calucation. Can you please help to clarify?
-
#define BRICK_VINSNS_SENSE_MAX_VOLTS ((float32_t)100)However, according to schematc VOSNS2_max should be 3.3(R20+R23)/R23 = 3.3 *(10+2.8)/2.8= 15.0857VWhy program and powersuite set it to 100V?If you look at #define BRICK_VOUT_SCALE ((float32_t) 3.3f / 4096.0f * (10.0f + 2.8f) / 2.8f), The Vout max used for calculating scale is correct. May we know where is 100V coming from?
2. The same question to VINSNS
#define BRICK_VINSNS_SENSE_MAX_VOLTS ((float32_t)100)
By calcuation the VIN max should be 60.46V
3. May we know how to calcuate Ipri max from schematic?
How do we get these value?