Part Number: TMS320F280041C
Greetings! I have F280041C and XDS110v3 probe and my project uses MotorControl_SDK_v5_04 as base. When I am using CCS 12 everything works just fine, but when I migrate to CCS 20.4 i can`t start debug my project. The UI never sets the pointer to my main(). When i start debug session my C28xx_CPU1 startus is disconnected, I manually connect it and I have a red dot right after C28xx_CPU1 and the status is halted. If i press continoue or step forward it just returns to the same state. The breakpoints in the mains are automaticly disable and i can`t reanable them. Can you tell me how to fix this?