Part Number: F29H85X-SOM-EVM
Hi,
F29h85x in HS-SE mode.
- By default, the post-build process generates a CPU1.bin file that includes CPU2.bin and CPU3.bin. In HS-SE mode, we intend to load CPU1 and CPU3 applications independently. We require guidance on modifying the post-build steps so that CPU1.bin includes only CPU2.bin, while CPU3.bin is generated as a separate image.
- CPU2 will not operate in lockstep with CPU1, and we plan to load the CPU2 application in FRI-1 RP0. Since CPU2.out is embedded within CPU1.out, we would like clarification on certificate generation:
Is a single certificate file (CPU1.cert.bin) generated after combining CPU2.out into CPU1.out, or does this file internally contain two separate certificates—one for CPU1 and one for CPU2?
Regards,
Shashank