Hello,
is there a Concerto VCU example available using C28x_VCU_LIB.lib ?
Customer wants to calculate CRC using library functions instead of using assembler code as described in the Concerto TRM.
Thank you in advance,
Mario
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
is there a Concerto VCU example available using C28x_VCU_LIB.lib ?
Customer wants to calculate CRC using library functions instead of using assembler code as described in the Concerto TRM.
Thank you in advance,
Mario
0601.F28M35x_VCU_CRC_Test_120207.zip
Hi Mario,
I have ported and attached the crc example from the VCU lib. I have tested on a F28m35h52c1 controlCARD. You will need f28m35x/v100 and VCU/v110 from controlSUITE to run this examples. If controlSUITE is not installed in the default location please change the macros.ini paths to the right location.
If you cant open the attachment let me know and i can send via email.