This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ezdsp F28335 ePWM5 and ePWM6



Hi,

I am using the DSP board F28335 and I am programming it using MATLAB blocks. I am working on a five phase machine and I need a 10 PWM pulses for the IGBTs. The first four PWMs ,ePWM1 (A&B), ePWM2 (A&B), ePWM3 (A&B) and ePWM4 (A&B), are working properly; but the fifith PWM is not working. I tried to use ePWM5 and ePWM6 to get the fifth PWM but there is no output on the pins of the dsp board. The code is right because it works on the other PWMs. Would someone please helps me solving this problem.

Thanks,

Mohamed