Part Number: AM263P4-Q1
Other Parts Discussed in Thread: TCA6424A, TCA6424
Hi Team,
I am working on the ADC module and testing the ADC SOC software example on AM263Px‑CC using AM263Px MCU+ SDK v11.01.00.
While running the ADC test example, I observe that the ADC output remains constant, even when I vary the input voltage from 0 V to 3.2 V applied to ADC0_AIN2 (HSEC pin 15).

Despite changing the input voltage, the ADC result does not change accordingly.
Questions:
- Is there a recommended way to properly test the ADC to obtain variable digital counts in the range 0 to 4095?
- Are there any specific configurations (SOC, reference voltage, pinmux, etc.) that I should verify for this example?
- Does the example use any internal connection or test signal that overrides the external pin input?
Any guidance on how to correctly validate ADC functionality on AM263Px would be appreciated.
Thanks in advance.