Part Number: CCSTUDIO-THEIA
Other Parts Discussed in Thread: TMS320F28379D, TMS320F28375D, SYSCONFIG, C2000WARE
Hi team,
I am not able to use the syscfg GUI tool to change the chip selection, default chip is TMS320F28375D, and i want to switch to TMS320F28379D, but the syscfg tool display nothing when i click on the drop-down arrow button, and all settings has gone. When I open syscfg again, CCS behaves the same way. Looks like this is a software bug and other users have reported this long ago but still not resolved. Earlier I was able to switch properly but now after some CCS update not able to do so. To make things worse, I am not able to switch to earlier CCS versions. If I open CCS v20.1, it is still opening CCS v20.4.1
CCS version: 20.4.1.4
Syscfg version: 1.26.0+4407
Compiler version: TI v22.6.3.LTS
Kindly help to resolve this critical issue or help in identifying in which CCS version or Syscfg version, this was working fine and how to switch to that.
Thanks,
Bhargav Saikia.