This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSHVMTRINSPIN: same issue but the forum is now closed without answer

  • The two LEDs are controlled by GPIO pins from MCU, so without loading correct software, the status of the LED means nothing...

    Please try to load the firmware or empty of the controlCARD Flash, then these two GPIOs should boot as high impedance, and will be at low (LED off) from the pull down resistor on the board design.

    Han