This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2612: AM261 PRU with Profinet and SPI running power consumption

Part Number: AM2612

Hi Team,

My customer is a lower power application, they don't need AM261 runing at a very high frequency, it just need running Profinet and SPI. I think both can running on PRU. So do we have some datas which can show PRU power consumption? it need lower than 0.5W.

what the minimum of PRU when need running profinet? 

Can we disable R5F core, and only let PRU running, what the power consumption?

our data sheet only show the maximum power consumption, what 's the minimum ?

Thanks

Best Regards,

Zane

image.png