Part Number: TMS320F28P659SH-Q1
Team,
I have seen this older post already:
https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/432344/difference-between-aio-and-gpio-pins-for-tms320f28027
Also I looked at:
-TRM www.ti.com/.../spruiz1 section "14.3 Digital Inputs on ADC Pins (AIOs)" and "17.4 Digital Inputs and Outputs on ADC Pins (AGPIOs)".
-Datasheet www.ti.com/.../sprsp69 section 5.5.2 Digital Inputs and Outputs on ADC Pins
Questions:
-Are there any drawback to use AIO or AGPIO pins instead of GPIO for a digital interface?
-For example could AIO / AGPIO pins be more prone to noise or lake accuracy? (apart from the high dv/dt use case listed in note of section 17.4)
-Are there some interface that are more sensitive to electrical signaling for which it is prefered to use a GPIO only pin?
-AIO are not listed in Datasheet Table 5-12 unused pins:
Does it mean that each AIO/AGPIO is associated with a GPIO and one of the acceptable practise for GPIO need to be used?
or is it better to select AGPIO (vs GPIO) for unused pins as it is by default disconnected?
Thanks in advance,
Anber