Part Number: CCSTUDIO-THEIA
Hi Team,
I am working with the TMS320F28P650DK6 controller and facing an issue with code retention after power cycling.
Issue description:
- I am able to successfully flash the program using CCS.
- The code runs correctly immediately after flashing.
- However, after powering OFF and then ON again, the program does not execute.
- This behavior is observed even when using the provided example projects (e.g., LED blink example).
Observations:
- Flashing process completes without errors.
- Code execution works only once (right after flashing/debug session).
- After reset or power cycle, the device does not seem to boot from flash.
What I have tried:
- Tested with TI example projects (LED blink).
- Reflashed multiple times.
- Verified connections and power supply.
Questions:
- Is there any specific configuration required to ensure the code runs from flash after power cycle?
- Could this be related to boot mode configuration or linker settings?
- Are there any additional steps needed to properly program flash memory on this device?
I would appreciate any guidance on resolving this issue.
Thanks in advance.